Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

2,789 次查看
harlenChen
Contributor I
We use the MC908QL4MDW.. But the logo on IC is MC908QL4MDW1? And sometimes, the logo is MC908QL4MDW2?  I want to konw the different??? I can not get the information about the '1' or '2' from the datasheet.
thx
Harlen
标签 (1)
0 项奖励
回复
1 回复

1,447 次查看
RockyRoad
Contributor III
Harlan -
 
There was a problem with a mask set that the internal clock would not trim to the 25.6 MHz option. These parts are marked with the '1'.  Parts that will trim correctly at 25.6 MHz are marked with '2'.
 
If you are using an external crystal or if you are using the internal at 4, 8, or 12.8 MHz, then this won't make a difference.
 
- Rocky
0 项奖励
回复