Hi,
I am using KDS2.0, KSDK 1.1.0 and Processor Expert on K64F Demo board. Everything is working fine...
Then I re-install the KDS 2.0 and KSDK1.1.0 and did updating for Processor Expert because the virus damage my IDE.
Now, I am trying to open the working project, give me lots of errors as below...But, I can build my project, but I can't use PE now...
"
Cannot create new item, could not load item: symbol = VersionSpecificItem item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_main.item
Cannot create new item, could not load item: symbol = SdkSpecificMethodsCPU item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_MK64F12_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_port_hal\Items\1.1.0-GA\fsl_port_hal_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_sim_hal\Items\1.1.0-GA\fsl_sim_hal_methods.item
Cannot create new item, could not load item: symbol = VersionSpecificItem item = Beans\fsl_os_abstraction\Items\1.1.0-GA\fsl_os_abstraction_main.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_os_abstraction\Items\1.1.0-GA\fsl_os_abstraction_methods.item
.......
"
Could anybody tell me how to install KDS 2.0 and KSDK 1.1.0 and PE properly?
Thanks,
Christie
Solved! Go to Solution.
Hello Christie Su:
Did you install the KSDK v1.1.0 Eclipse Update. If not please follow the attached guide.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Christie Su:
Did you install the KSDK v1.1.0 Eclipse Update. If not please follow the attached guide.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jorge,
Yes. I did updating. But, I didn't use *.zip file because there is no this file under KSDK1.1.0 and there are only jar files...
Thanks,
Christie
Hello Christie,
You can find work instruction in the document How to install Kinetis SDK 1.1.0 support in KDS 2.0.0, see the link:
https://community.freescale.com/docs/DOC-104206
Best Regards,
Marek Neuzil
Hi,
After I uninstall the KSDK 1.1.0 Eclipse Update from About Installation Windows, then, re-install the KSDK1.1.0 Eclipse Update using the suggested way, it works now...
Thank you for your help!
Christie
Hi Christie,
Does your KSDK directory like this :
If not , maybe the KSDK1.1.0 does not install successfully.
While it doesn't matter , you can also update KSDK online. please do as this :
Help-> Install New Software
then :
refer to the reminder to install it .
Best Regards,
Alice
------------------------------------------------------------------------------------------
If this post answers your question, please click the Correct Answer button.
-----------------------------------------------------------------------------------
If this post help your question, please click the helpful Answer button.