Hi,
I am using KDS2.0, KSDK 1.1.0 and Processor Expert on K64F Demo board. Everything is working fine...
Then I re-install the KDS 2.0 and KSDK1.1.0 and did updating for Processor Expert because the virus damage my IDE.
Now, I am trying to open the working project, give me lots of errors as below...But, I can build my project, but I can't use PE now...
"
Cannot create new item, could not load item: symbol = VersionSpecificItem item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_main.item
Cannot create new item, could not load item: symbol = SdkSpecificMethodsCPU item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_MK64F12_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_clock_manager\Items\1.1.0-GA\fsl_clock_manager_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_port_hal\Items\1.1.0-GA\fsl_port_hal_methods.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_sim_hal\Items\1.1.0-GA\fsl_sim_hal_methods.item
Cannot create new item, could not load item: symbol = VersionSpecificItem item = Beans\fsl_os_abstraction\Items\1.1.0-GA\fsl_os_abstraction_main.item
Cannot create new item, could not load item: symbol = SdkSpecificMethods item = Beans\fsl_os_abstraction\Items\1.1.0-GA\fsl_os_abstraction_methods.item
.......
"
Could anybody tell me how to install KDS 2.0 and KSDK 1.1.0 and PE properly?
Thanks,
Christie
已解决! 转到解答。
Hello Christie Su:
Did you install the KSDK v1.1.0 Eclipse Update. If not please follow the attached guide.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Christie Su:
Did you install the KSDK v1.1.0 Eclipse Update. If not please follow the attached guide.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Christie,
You can find work instruction in the document How to install Kinetis SDK 1.1.0 support in KDS 2.0.0, see the link:
https://community.freescale.com/docs/DOC-104206
Best Regards,
Marek Neuzil
Hi,
After I uninstall the KSDK 1.1.0 Eclipse Update from About Installation Windows, then, re-install the KSDK1.1.0 Eclipse Update using the suggested way, it works now...
Thank you for your help!
Christie
Hi Christie,
Does your KSDK directory like this :
If not , maybe the KSDK1.1.0 does not install successfully.
While it doesn't matter , you can also update KSDK online. please do as this :
Help-> Install New Software
then :
refer to the reminder to install it .
Best Regards,
Alice
------------------------------------------------------------------------------------------
If this post answers your question, please click the Correct Answer button.
-----------------------------------------------------------------------------------
If this post help your question, please click the helpful Answer button.