Hi ,
We have gone through all the device tree and forums,
i.mx6q Enable Dual Display of Ubuntu
imx6q dual display LVDS +HDMI has problem `
We have the DUAL lvds clone mode already working but we want LVDS + HDMI to work in clone mode.
Any help on this regards will help,
Thanks,
-Rick.
Hi Rick
unfortunately such case is not supported in nxp bsps, maybe helps attached experimental patch for L3.0.35,
display cloning use case for i.MX6DQ SabreAI: sending the same IPU DI content to LVDS and HDMI, in the same time.
For example, have IPU0 DI0 to drive both LDB and HDMI.
Video parameters should be: video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24 ldb=sin0 video=mxcfb1:dev=hdmi,1024x768@60,if=RGB24
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Could you please comment on the status of such use case (IMX6Q clone LVDS/LCD display to HDMI) in the recent NXP 4.14.78 BSP? Does it have such use case?
Thanks!
Regards,
Sergei
Hi Sergei
no it is not officially supported.
Best regards
igor
i have the same problem. my kernel 3.0.35,cpu imx.6Q, QT4.8.5; i get the patch,but it can not disaply in the same time.
I'm sorry for being so stubborn, but here is what I see in the Android N7.1.2_2.0.0 Release notes document, Table 2 "Features":
...
UI (dual display,
LVDS+HDMI, UI
mirror displayed
on second
device)
...
This feature is supported on the IMX6Q boards for Android, out-of-box.
Could please someone explain, on the technical level, what needs to be done in the Linux kernel to get the LCD/HDMI mirrored mode working on Linux? Perhaps, I need to configure IPU to use the same ipu_id and display_id for both controllers?
dual display is described in sect.3.4.3 Booting with dual displays: LVDS and HDMI displays
attached Android_Quick_Start_Guide.pdf found on
Best regards
igor