Hi everyone,
I'm using the CodeWarrior V6.2 to program a MC9RS08KA2 (2 KB Flash).
I'm also using a "USB Multilink" of P&E Micro (www.pemicro.com).
When I choose "P&E Multilink/Cyclone Pro", the window "PEMICRO Connection Manager" is open and the first field to be choosed is "Interface".
My problem is: if I create a new project by choosing a uC of HCS08 family, I have in this field the option: "USB HCS08/HCS12/CFV1 Multilink - USB Port". In this case, the hardware is correctly detected by the CodeWarrior.
However, as I really need to create a new project by choosing the uC MC9RS08KA2, I don't have anymore the option above, but "USB HCS08/HCS12/CFV1 Multilink (Rev C or Later)".
In this case, my USB Multilink is not detected!!!
Please, does anyone know what I can do to have the USB Multilink detected in this case?
Thank you, in advance.
Cremonezi
Solved! Go to Solution.
Dear cremonezi,
I supect that your BDM does not support the RS08 chips. These require a 12V supply for programming which is absent in the earlier versions of the P&E BDMs (before RevC?). Is your BDM this version?
I suggest you check the P&E website or contact them by email to check this.
bye
Dear cremonezi,
I supect that your BDM does not support the RS08 chips. These require a 12V supply for programming which is absent in the earlier versions of the P&E BDMs (before RevC?). Is your BDM this version?
I suggest you check the P&E website or contact them by email to check this.
bye
Hi pgo,
Thank you very much for your answer.
I've contacted the technical support from pemicro.com and you are right.
I have actually a USB-ML-12 Rev B, which does not support the RS08 family.
Best regards,
Cremonezi