Debug u-boot SPL on NXP imx8mm-evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug u-boot SPL on NXP imx8mm-evk

3,059 Views
sne555
Contributor I

Hello,

How to debug u-boot SPL on i.MX8M Mini (NXP imx8mm-evk) ?

Why the $pc goes to 0x200 instead of executing spl instruction ?

```

user@desktop:~/sources/u-boot$ ../binutils-gdb/gdb/gdb -q spl/u-boot-spl
Reading symbols from spl/u-boot-spl...
(gdb) target remote :3333
Remote debugging using :3333
0x000000000000c904 in ?? ()
(gdb) load
Loading section .text, size 0x101c8 lma 0x7e1000
Loading section .rodata, size 0x23a3 lma 0x7f11c8
Loading section .data, size 0x5f80 lma 0x7f3570
Loading section .u_boot_list, size 0x1400 lma 0x7f94f0
Start address 0x00000000007e1000, load size 104683
Transfer rate: 69 KB/sec, 11631 bytes/write.
(gdb) i r pc
pc             0x7e1000            0x7e1000 <_start>

(gdb) x/i 0x7e1000
   0x7e1000 <_start>:    b    0x7e1028 <reset>

(gdb) stepi
0x0000000000000200 in ?? ()
(gdb) i r pc
pc             0x200               0x200

(gdb) x/i 0x200
=> 0x200:    b    0x13dc4

```

BOOT_MODE[3:0] = 0101 (serial downloader)

openocd 0.10.0 (openocd -f ./tcl/interface/ftdi/olimex-arm-usb-ocd-h.cfg -f ./tcl/board/imx8mp-evk.cfg)

GNU gdb (GDB) 10.0.50.20200418-git

Best regards

Labels (1)
0 Kudos
Reply
7 Replies

2,258 Views
iyun
Contributor I

Everyone has the same problem. Who has the solution

0 Kudos
Reply

2,947 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You some comments.

Regards,

Yuri.

0 Kudos
Reply

2,586 Views
joaze
Contributor I

Hi Yuri!

I have similar problems on a imx8mn-evk board when I try to load the SPL.

What was the solution to the https://community.nxp.com/t5/i-MX-Processors/Debug-u-boot-SPL-on-NXP-imx8mm-evk/m-p/1079629 question.

0 Kudos
Reply

2,258 Views
iyun
Contributor I
Everyone has the same problem. Who has the solution
0 Kudos
Reply

2,565 Views
Yuri
NXP Employee
NXP Employee

@joaze 
Hello,

   Last time I sent some material how to debug the issue. I do not know 
exact solution. You can create separate thread for considerations.

Regards,
Yuri

0 Kudos
Reply

2,676 Views
ilko
Contributor I

Yuri,
Do you have a solution for the problem?

0 Kudos
Reply

2,923 Views
davidwang66
Contributor I

We got same issue. Could you pls email info to us. 

Thanks

0 Kudos
Reply