Hello,
I wanted to evaluate Android on the i.MX7Dual Sabre evaluation board and it's LCD panel (LCD8000-43T).
Is there a know software configuration (Android demo release) that works out the box?
By 'works out of the box' I mean that the Android UI should be displayed on the a monitor, without requiring any additional configuration or build.
I ask this because I recently purchased i.MX7ULP evaluation kit (MCIMX7ULP-EVK) and it's MIPI DSI display (TFT3P5581-T). But when I flash the Android P9.0.0_2.2.0 prebuilt image from NXP, I don't see any thing on the display. Furthermore, there is no display using standard HDMI monitors either. This might be because this is a relatively new board and the software release is also recent and some things might not be implemented or may be buggy. I have raised a support ticket to NXP regarding this.
So can someone tell me about their experience with i.MX7Dual Sabre + Android BSP image.
If you have a known working configuration then please let me the following details:
-The exact Android release that is known to be working (link will be appreciated).
-The display that was used (HDMI or LCD).
-Whether touch support (for LCD) worked out of the box.
-Any boot-loader configuration that may be required or useful.
Thanks a lot.
Solved! Go to Solution.
Hello Adwait,
MX7D work with android Things with MIPI WVGA TFT3P5581. More info:
https://developer.android.com/things/hardware/imx7d
Regards
Hello Adwait,
MX7D work with android Things with MIPI WVGA TFT3P5581. More info:
https://developer.android.com/things/hardware/imx7d
Regards
This is for the PICO-IMX7 board from TechNexion.
I am looking for an evaluation board directly from NXP - or one with open hardware schematics.
Thanks for your help anyways.