Hi,
I use the Codewarrior for MC68HC908gz8 and I installed the codewarrior V11.0 and It doen't have the MC68HC908gz8. How I use MC68HC908gz8 with codewarrior ?
I have the licence for codewarrior V6.3 but doen't work with windows 10.
Best regards.
Gilmar
Hi,
MC68HC908gz8 is HC08 device which is only supported by CW6.3.
CW6.3 doesn't support 64bit win7/10 platform.
the officially recommendation is using CW6.2 on 32bit windows xp.
We have user provide unofficial method of install CW6.3 on win10 64bit.
How-to Directly Install CodeWarrior 6.3 Classic in Windows 7 and 10 x64 (Unofficial Method)
You can refer it but NXP doesn't provide technical support of it. Thanks for your understanding.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thank you.
I installed and is work well.
Best regards.
*Gilmar Ribeiro de Oliveira *
Supervisor de Engenharia de Pesquisa e Desenvolvimento - P&D
Tel: 55 35 3471.2555 Ramal: 0218
gilmar@mg.sense.com.br www.sense.com.br
Av. Joaquim Moreira Carneiro, 600 - Santana
CEP: 37540-000 - Santa Rita do Sapucaí/MG Brasil
Em 22/11/2018 01:59, ZhangJennie escreveu:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: Codewarrior for MC68HC908GZ8
reply from ZhangJennie
<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread>
in /CodeWarrior Development Tools/ - View the full discussion
<https://community.nxp.com/message/1083038?commentID=1083038&et=watches.email.thread#comment-1083038>
>
You are welcome.