I'm playing with the EWM driver example provided with the FRDMK64 SDK for MCUXpresso. The example itself runs fine, but i'm trying to map EWM_Out. I've used MCUXpresso's Pin Tool to generate the code to configure PTE24 to EWM_Out and copy/pasted the generated code into the respective pin_mux.c/.h files included in the board folder of the frdmk64f_ewm project. The project builds fine, but when i run the debugger it halts at the HardFault_Handler. When stepping thru the code, prior to halt, it appears the fault occurs when attempting to configure PTE24. Specifically when the PCR is configured in the Port_SetPinMux function.
**********************************
Here is the code generated by Pin Tools...
pin_mux.h **************
/*! @name PORTE24 (number 31), J2[20]/U8[4]/I2C0_SCL
@{ */
#define BOARD_INITPINS_ACCEL_SCL_PORT PORTE /*!<@brief PORT device name: PORTE */
#define BOARD_INITPINS_ACCEL_SCL_PIN 24U /*!<@brief PORTE pin index: 24 */
/* @} */
pin_mux.c **************
/* PORTE24 (pin 31) is configured as EWM_OUT_b */
PORT_SetPinMux(BOARD_INITPINS_ACCEL_SCL_PORT, BOARD_INITPINS_ACCEL_SCL_PIN, kPORT_MuxAlt6);
*************************************
I have not changed anything else from the default EWM configuration set in the driver example.
I read something in the K64 Reference Manual about "The pad state is controlled by the EWM_Out signal only after the EWM is enabled by the EWMEN bit of the CTRL register." I don't know if this is just information or if it means the IO pin cannot be configure to EWM_Out until after EWM is enabled. In the driver example, the IO pin is configured prior to EWM being enabled.
Am I missing a configuration parameter or sequence somewhere?
Hi Kevin
Try enabling the Port E gate (0x00002000) in SIM_SCGC5 before accessing its configuration register.
Regards
Mark
uTasker - for more performance and faster, cheaper product development