Hi All,
I have an T2080-RDB board,
i am a beginner for this board .
i have to perform post tests(RAM,PROM and Ethernet) on the board,
any suggestion to perform the test would be appreciated .
Hello Anshul khare,
You could refer to the following configuration in include/configs/P2041RDB.h to configure post memory test.
#define CONFIG_POST CONFIG_SYS_POST_MEMORY /* test POST memory test */
#define CONFIG_SYS_MEMTEST_START 0x00200000 /* memtest works on */
#define CONFIG_SYS_MEMTEST_END 0x00400000
#define CONFIG_SYS_ALT_MEMTEST
#define CONFIG_PANIC_HANG /* do not reset board on panic */
Please refer to "Memory test" section in post/tests.c, the function memory_post_test is used to do memory test with software method, which is defined in post/drivers/memory.c.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------