I am a Ubuntu 16.04 development host and installed the Segger tools. I have connect the eval board port J28 and the mass storage device appears. I can load up designer loads by dragging and dropping. All settings on the board are default and it is using HyperFlash. When I try to start the JLinkGDBServer it does not see the target. What steps am I missing?
Here's my "DETAILS.TXT"
# DAPLink Firmware - see https://mbed.com/daplink
Unique ID: 0227000041114e450031300cc40300555ab1000097969900
HIC ID: 97969900
Auto Reset: 0
Automation allowed: 0
Overflow detection: 0
Daplink Mode: Interface
Interface Version: 0244
Bootloader Version: 0242
Git SHA: 853df431d81359e822f49363891f877f17d31efb
Local Mods: 0
USB Interfaces: MSD, CDC, HID
Bootloader CRC: 0x73707d49
Interface CRC: 0x565000e7
Remount count: 0
Here's the output from JLinkGDBServer
$ ./JLinkGDBServer
SEGGER J-Link GDB Server V6.32d Command Line Version
JLinkARM.dll V6.32d (DLL compiled May 28 2018 16:58:57)
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: off
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: Unspecified
Target interface: JTAG
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
Connecting to J-Link failed. Connected correctly?
GDBServer will be closed...
Shutting down...
Could not connect to J-Link.
Please check power, connection and settings.kannhild@natubuntu01:
After loading OpenSDA 2.1 the Segger gdbserver now connects and works find. But now my mass storage flash downloader no longer works... What is the best way to download to flash when running OpenSDA 2.1?
Hi,
after you upgrading OpenSDA interface. What's your GIT SHA number and SDK version?
they must match each other.
If you use latest OpenSDA, you need use SDK2.3.1 or later.
i.MX RT1050 CMSIS-DAP drag-and-drop programming
https://community.nxp.com/docs/DOC-340762
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------