SDK_2_x-FRDM-KE04Z - Import wizard - No examples to import

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK_2_x-FRDM-KE04Z - Import wizard - No examples to import

2,679 Views
george_ch
Contributor II

MCUEpresso IDE v10.1.1

With the downloaded and installed (default) boards:-  SDK_2_x-FRDM-KE04Z  Ver 2.3.0

When using the MCUEpresso IDE   'SDK import wizard'

I'm seeing No examples to import listed

(and therefore unable to continue)

The above SDK has examples in its folders

Please advise.

0 Kudos
Reply
3 Replies

2,485 Views
george_ch
Contributor II

Thanks Alice.

One serial port example now found.

A few more would be helpful.

BR

George

0 Kudos
Reply

2,485 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello George,

Development expert said

“the resource is very limited in FRDM-KE04Z, so all of our SDK examples cannot even succeed build for MCUXpresso IDE. So, FRDM-KE04Z does not support MCUXpresso IDE.”

I checked other toolchain SDK package, for example KDS, IAR or MDK, they includes demo code,

I think you can create a new proejct on MCUXpresso IDE, then refer to the demo code on other IDEs.

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,485 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello George Chamberlayne ,

Thanks for your sharing, I will report it to development team.

BR

Alice

0 Kudos
Reply