SDK_2_x-FRDM-KE04Z - Import wizard - No examples to import

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK_2_x-FRDM-KE04Z - Import wizard - No examples to import

1,810件の閲覧回数
george_ch
Contributor II

MCUEpresso IDE v10.1.1

With the downloaded and installed (default) boards:-  SDK_2_x-FRDM-KE04Z  Ver 2.3.0

When using the MCUEpresso IDE   'SDK import wizard'

I'm seeing No examples to import listed

(and therefore unable to continue)

The above SDK has examples in its folders

Please advise.

0 件の賞賛
返信
3 返答(返信)

1,616件の閲覧回数
george_ch
Contributor II

Thanks Alice.

One serial port example now found.

A few more would be helpful.

BR

George

0 件の賞賛
返信

1,616件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello George,

Development expert said

the resource is very limited in FRDM-KE04Z, so all of our SDK examples cannot even succeed build for MCUXpresso IDE. So, FRDM-KE04Z does not support MCUXpresso IDE.

I checked other toolchain SDK package, for example KDS, IAR or MDK, they includes demo code,

I think you can create a new proejct on MCUXpresso IDE, then refer to the demo code on other IDEs.

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,616件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello George Chamberlayne ,

Thanks for your sharing, I will report it to development team.

BR

Alice

0 件の賞賛
返信