I have enabled SPL_BUILD in uboot and it compiles ok, I configure DDR parameters in sabresd.c file just like my DCD (that works) but SPL doesn't boot ( at least I can't see any log in console). My questions are:
1. Printf works in SPL to generate log?
2. How SPL finds uboot.
3. I have to write to SdCard SPL file and uboot.img? Which seek I have to use in DD?
4. Uboot from freescale works SPL only enabling SPL_BUILD?
Hi Leonardo
nxp uboot does not use spl
uboot-imx.git - Freescale i.MX u-boot Tree
one can post this on uboot mail list
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor, thanks for your answer. Only a doubt in the sabresd file http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sabresd/mx6sabresd.c...
At line 374 and 1320 there are configs for SPL, this not work?
Hello Leonardo,
I've met the question as you too.(https://community.nxp.com/message/864563 ) Do you solve it? If yes, could you show me some details? Thanks.
Best wishes,
Mc
please check
https://community.freescale.com/message/402940#402940
this option is not used in nxp uboot, though it is present in codes.
One can also post this to meta-fsl-arm mailing list, so that someone familiar with it
could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor