Hi All,
I am working on Marshmallow and kernel 4.1.
Currently I have an issue which is everytime I enter a number in a dialer I get pop up saying Unfortunately, Phone has stopped. Seems like the dialer app is the culprate but I am not sure where to start from on this.
Here are my adb logcat attached
Original Attachment has been moved to: temp.txt.zip
Solved! Go to Solution.
Hi Ali
one can try to debug it using AN4553 Using Open Source Debugging Tools for
Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I have tried that but somehow its not working for me. Is there anything else you can recommend.
Regards
Ali
Hi,
Just an update on this. It is solved had wrong DPI settings
Hi Igor,
Thanks for the quick reply. I am currently looking at this will update once done.
Regards
Ali