Hi,
I am trying to build images for IMX6Q-SDB board using Yocto.
I have followed below steps.
#mkdir ~/bin
#curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
The above curl command failed so downloaded repo from brpwser and saved to ~/bin.
#chmod a+x ~/bin/repo
#export PATH=~/bin:$PATH
#mkdir fsl-release-bsp
#cd fsl-release-bsp
#git config --global user.name "Your Name"
#git config --global user.email "Your Email"
#git config --list
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
The repo init command failed while trying to access "https://gerrit.googlesource.com/git-repo/info/refs"
Get https://gerrit.googlesource.com/git-repo/clone.bundle
Get https://gerrit.googlesource.com/git-repo
error: Failed connect to gerrit.googlesource.com:8002; Connection timed out while accessing https://gerrit.googlesource.com/git-repo/info/refs
fatal: HTTP request failed
I tried to access "https://gerrit.googlesource.com/git-repo/info/refs" through browser then it is giving page not found error.
I have tried with repo from "http://commondatastorage.googleapis.com/git-repo-downloads/repo", but still same error.
Can you please guide me whether the repo I am using is proper or not.
Solved! Go to Solution.
The issue is with the proxy. In office networy we are using proxy, after disabling proxy using "unset http_proxy" it is working fine.
We can disable proxy in /etc/environment also.
After repo init command repo sync also succeeded.
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
#repo sync
Following commands are used to build images using yocto for IMX6 Sabersd.
#source setup-environment build
#bitbake core-image-minimal
The issue is with the proxy. In office networy we are using proxy, after disabling proxy using "unset http_proxy" it is working fine.
We can disable proxy in /etc/environment also.
After repo init command repo sync also succeeded.
#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
#repo sync
Following commands are used to build images using yocto for IMX6 Sabersd.
#source setup-environment build
#bitbake core-image-minimal