We are building a custom board with an LS1020a processor and an attached N25Q256 QSPI flash. The target tasks/flash programmer interface shows the N25Q128 (which I have used on the TWR dev board) and the N25Q512. I found this document on how to add a flash chip to CW 10: Adding a new Flash Device to Codewarrior 10.x
When I navigate to the xml files described in that doc, I see that for algorithm, the N25Q128 uses N25Q128_QSPI.elf. Can I use this .elf as well for the N25Q256? I would provide a new xml file and modify the manifest as described in DOC_94792.
Interestingly, the N25Q512 xml file calls out N25Q512_QSPI.elf as it's algorithm, but no such file was installed in my CW installation.
Solved! Go to Solution.
N25Q128_QSPI.elf algorithm can be used with the mention that protect and unprotect action will not works correctly. But, erase/program/dump should works well.
You have to create a new XML, with the correct configuration for the new device.
Adrian
N25Q128_QSPI.elf algorithm can be used with the mention that protect and unprotect action will not works correctly. But, erase/program/dump should works well.
You have to create a new XML, with the correct configuration for the new device.
Adrian