Hello, could you confirm the temperature absolute max rating specified in the MPC8245 datasheet ?
The value is currently 105°C, the same a the recommended value. Usually there is some margin between those 2 values.
Thanks for your help.
Best regards,
Stéphane
Have a great day,
Yes, operational die-junction temperature range in the Absolute Maximum Ratings and Die-junction temperature in the Recommended Operating Conditions are the same.
Notice that for the next power processor generations like MPC83xx, MPC85xx they provide only Storage temperature range in the Absolute Maximum Ratings, while the maximal die junction temperature limits the Recommended Operating Condition.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------