Hello,
I have Imx6Q with android 4.2
I am trying to connect a non-standard display with a resolution of 640 by 240.
Connect it by LCD TTL.
Horizontal Sync of my monitor is 15.38 kilohertz.
All modes are registered in modedb.c start from 31.5 kHz.
I know that Linux have /etc/X11/xorg.conf where you can set the range from where to where.
Where to change the Horizontal Sync on Android?
I tried to create a new driver in the video / mxc / and write it in mxc_lcdif.c, after starting the FB the resolution changes but the Horizontal Sync remains the same or even displays nonsense
I would be grateful for any help and tips.
Andrey.