About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP

Jump to solution
1,237 Views
yuuki
Senior Contributor II

Dear all,


Our customer wants to make a system using i.MX6Solo and PF0100.
They are going to wake-up a system by an Ethernet.


I have the following several questions.

1)
According to section "23.5.7.1 Sleep mode"(P.1132) of a reference manual, the following is explained.
"In addition, when the processor is in Stop mode, Sleep mode is entered, without affecting the ENETn_ECR register bits.

When a processor is Standby or Deep Sleep mode, can MAC enter a Sleep mode?


2)
They use LinuxBSP.
Is there a sample cord for a system to be waked-up by a Magic packet of Ethernet?


Best Regards,
Yuuki

Labels (1)
Tags (6)
0 Kudos
Reply
1 Solution
929 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

official linux BSP does not support wake on lan, however

there is Community patch below

Wake on lan in mx6 sabresd board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
930 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

official linux BSP does not support wake on lan, however

there is Community patch below

Wake on lan in mx6 sabresd board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply