LVDS to HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS to HDMI

16,669 Views
pankajrana
Contributor III

Hello,

I would like to inquire on the possibility of LVDS to HDMI conversion. OK, I'll go into the details.

For one existing board - i.Mx6 Quad , supports one HDMI, but as per requirement, an additional HDMI monitor needs to be supported. For this we have thought of LVDS to HDMI conversion.

Current Approach:

LVDS Connector output2nd HDMI connector i/p
LVDS_TX0 +/-HDMI_D0 +/-
LVDS_TX1 +/-HDMI_D0 +/-
LVDS_TX2 +/-HDMI_D0 +/-
LVDS_clk +/-HDMI_clk +/-

Remaining signals (I2C, etc) are taken care of , with similar settings as required for HDMI.

For the current approach we have planned for a customized wiring, and no usage of any converter. So any possible outcome of this experiment ??

Any feedback/reply will be highly appreciated.

Thanks.

-Pankaj Rana

Labels (2)
0 Kudos
Reply
2 Replies

4,286 Views
sathiyan_durai
Contributor I

You have any adapter board supports LVDS to HDMI? Takes only LVDS Input signals and power.

Thanks

Sathiyan

0 Kudos
Reply

4,286 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

though electrically these interfaces may be connected,

lcd data/sync mapping is different and not transparent.

For example HDMI stream may embed audio data.

There are lvds-hdmi converters, for example below

CH7036

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------