Hello,
I would like to inquire on the possibility of LVDS to HDMI conversion. OK, I'll go into the details.
For one existing board - i.Mx6 Quad , supports one HDMI, but as per requirement, an additional HDMI monitor needs to be supported. For this we have thought of LVDS to HDMI conversion.
Current Approach:
LVDS Connector output | 2nd HDMI connector i/p |
---|---|
LVDS_TX0 +/- | HDMI_D0 +/- |
LVDS_TX1 +/- | HDMI_D0 +/- |
LVDS_TX2 +/- | HDMI_D0 +/- |
LVDS_clk +/- | HDMI_clk +/- |
Remaining signals (I2C, etc) are taken care of , with similar settings as required for HDMI.
For the current approach we have planned for a customized wiring, and no usage of any converter. So any possible outcome of this experiment ??
Any feedback/reply will be highly appreciated.
Thanks.
-Pankaj Rana
You have any adapter board supports LVDS to HDMI? Takes only LVDS Input signals and power.
Thanks
Sathiyan
Hi Pankaj
though electrically these interfaces may be connected,
lcd data/sync mapping is different and not transparent.
For example HDMI stream may embed audio data.
There are lvds-hdmi converters, for example below
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------