hi guys..
want to ask..why my trkmpc560xb when connected to power supply, the RSTLED is on..it is broken or something..?
tq
Solved! Go to Solution.
Hello fahmirazak
I hope your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.
Depending if you can program you mcu, is if it is broken.
Regards,
Hello fahmirazak
I hope your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.
Depending if you can program you mcu, is if it is broken.
Regards,
The same thing happens to me but once i flash it the led goes off, then when i plug it again to a source power tsomethimes the led goes on again, But it just happens on some programs that i flash i think (I hope) that it is a register that is corrupted or something
Mine is a mpc5606b
Can you flash it?
murraystewart-b04629 do you have 2 min to check this out? maybe you have an answer to this.
Thanks
cant flash..do you have any idea?