Hello,
My Name is Oscar and I'm trying to create a Project for my custom borad using MQX 4.1. I'm using codewarrior 10.5.
I clone the TWR-K60F120M (it suits to my custom board pretty well). The cloning process is done using the clone wizard from freescale (installed with MQX 4.1). There are no problems on the process itself, and after the process is done I can build the libraries with no problems. But when I want to creata a new MQX 4.1 project for my custom board, it does not appear in the list of available devices.
What I did wrong? How can I solve that?
Thanks in advances!
Oscar.
Solved! Go to Solution.
Hi Oscar,
please refer to https://community.freescale.com/message/356271#356271
I think that may be helpful.
B.R
XWP
Hi Oscar,
please refer to https://community.freescale.com/message/356271#356271
I think that may be helpful.
B.R
XWP
Hi Weiping Xu,
It worked.
Many thanks.
Oscar