HI
Anyone know why using the USB TAP ONCE unit and setting BP instead of showing me the code at the BP marker the debugger jump to internal interrupt?
Picture attached.
I tried using PEmicro Multilink Universal instead and it run OK.
I had the same problem with 2 USB TAO units I tested (revB)
I even tried to reset the USB TAP unit according to the manual instructions, but it did not help.
TIA
Please delete .metadata folder of workspace of CW 10.5.
Then reopen the project in CodeWarrior, and click on 'Project' menu-> Clean to remove the old object file, and then rebuild the project. Is the problem fixed?
Dear Fiona,
As you found out, there is a bug with the USB TAP ONCE that cause it.
Thank you for confirming it on the S/R, it's a pity that you don't publish this fact here to prevent community users to waist time on such bug.