Hi all,
I'm using fsl Gnome release on imx233. I build it with all gstreamer plugins and fsl multimedia codecs and libs.
totem plays the audio, but no video on screen. If I use gplay it plays both video and audio smoothly. But I want to use my device standalone, and hence need to launch it from the device using the tough screen.
Please, any hint would be appreciated.....
Aren´t you using Ubuntu rootfs from FSL site? I supposed you was.
Yes, I suppose Totem is using default video sink, I only don´t know which video sink is the default one =P
For screen size, I mean the totem window dimension. Try to use totem maximized.
Totem is using the default video sink, I guess
What do you mean by Ubuntu binary? .... (i'm using imx233 on a custom board btw.)
My screen resolution is 320x240, (3.5" TFT)
The fsl command line player shows almost the same log, but it plays smoothly rendering high quality video!
It is decoding movie too but this is not showing on screen. I think the issue is on videosink totem uses. Do you know which video sink totem uses?
Is there some new Ubuntu binary you can donwload?
Another thing I just remembered. How small is your totem screen? I know some codec (in fact, I don´t know if it´s for decoder or video sink) cannot handle very small windows screens (I thinks it´s because the resize ratio for IPU)
I don´t have anything else to add =(
Hi Daiane,
I connected my device to a PC rs-232 terminal and got the following log when I launch totem using the GUI on device. I opened from there a 3min mp4 video (MPEG-4, AAC), which plays well with 'gplay' on another rootfs.
< I can hear the audio clearly, but all I can see is a black window on the LCD.>
.
.
.
MFW_GST_V4LSINK_PLUGIN 1.8.0 build on May 31 2011 18:26:42.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs
** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/jamendo/jamendo.totem-plugin', Totem was not compiled with Python support
** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/jamendo/jamendo.totem-plugin
** (totem:925): WARNING **: Failed to create dbus proxy for org.gnome.SettingsDaemon: Could not get owner of name 'org.gnome.SettingsDaemon': no such name
** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/coherence_upnp/coherence_upnp.totem-plugin', Totem was not compiled with Python support
** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/coherence_upnp/coherence_upnp.totem-plugin
** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/opensubtitles/opensubtitles.totem-plugin', Totem was not compiled with Python support
** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/opensubtitles/opensubtitles.totem-plugin
** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/pythonconsole/pythonconsole.totem-plugin', Totem was not compiled with Python support
** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/pythonconsole/pythonconsole.totem-plugin
** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/youtube/youtube.totem-plugin', Totem was not compiled with Python support
** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/youtube/youtube.totem-plugin
MPEG4PARSER_06.01.08 build on Mar 3 2010 17:08:43.
MFW_GST_MP4_PARSER_PLUGIN 1.8.0 build on May 31 2011 18:26:37.
File is seekable
specific info size is: 2
specific info size is: 32
BLN_MAD-MMCODECS_AACD_ARM_03.05.00 build on Nov 25 2009 15:00:47.
MFW_GST_AAC_PLUGIN 1.8.0 build on May 31 2011 18:26:24.
MPEG4_ASP_D_01.02.01 build on Sep 27 2009 11:03:16.
MFW_GST_MPEG4ASP_DECODER_PLUGIN 1.8.0 build on May 31 2011 18:26:33.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs
successfully seek audio the track 1
successfully seek video the track 0
[V4L Update Display]: left=0, top=0, width=320, height=240
(totem:925): GStreamer-CRITICAL **: gst_structure_set_value: assertion `IS_MUTABLE (structure)' failed
>>V4L_SINK: Actually buffer status:
hardware buffer : 7
software buffer : 0
xcontext: width=320, height=240
>>V4L_SINK: Set max lateness = 2000000000.
DAC underflow detected
DAC overflow detected
...
< here it played a 3min mp4 encoded video, but only audio working>
...
Total rendered:0
>>V4L finalize: class finalized.
MPEG4PARSER_06.01.08 build on Mar 3 2010 17:08:43.
MFW_GST_MP4_PARSER_PLUGIN 1.8.0 build on May 31 2011 18:26:37.
File is seekable
specific info size is: 2
specific info size is: 32
BLN_MAD-MMCODECS_AACD_ARM_03.05.00 build on Nov 25 2009 15:00:47.
MFW_GST_AAC_PLUGIN 1.8.0 build on May 31 2011 18:26:24.
MPEG4_ASP_D_01.02.01 build on Sep 27 2009 11:03:16.
MFW_GST_MPEG4ASP_DECODER_PLUGIN 1.8.0 build on May 31 2011 18:26:33.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs
MFW_GST_V4LSINK_PLUGIN 1.8.0 build on May 31 2011 18:26:42.
successfully seek audio the track 1
successfully seek video the track 0
[V4L Update Display]: left=0, top=0, width=320, height=240
(totem:925): GStreamer-CRITICAL **: gst_structure_set_value: assertion `IS_MUTABLE (structure)' failed
>>V4L_SINK: Actually buffer status:
hardware buffer : 7
software buffer : 0
xcontext: width=320, height=240
>>V4L_SINK: Set max lateness = 2000000000.
Waiting for your reply....
Daniel.
anybody there?... please help. I couldn't solve this.
Thanks in advance