To help you find solutions to problems that have already been solved, we have posted this message. It contains an entire topic ported from a separate forum. The original message and all replies are in this single message.
Posted: Jun 04, 2005 - 09:49 AM
Hi,
I'm just beginning to develop an mc9s12dp256 via Wytec's Dragon12 Dev board. Admittedly I'm fairly new to C as well.
I'm using a demo version of CW12V3_1.
I'd like to set DDRB to 0xFF and PORTB to 0xFF (to turn on some LED's associated with port b)
I've started a new project using the _Dx256_L91N project stationary.
I explored the header S12CPU15V1_5.h which defines the ports but I can't figure out what code to write to set the values.
I have been successful in downloading and launching sample programs from the RAM via DBug12. But they were based on a different stationary.
Any help would be greatly appreciated! Thanks.
Posted: Jun 08, 2005 - 11:41 AM
Hi,
I would suggest that you use "new project wizard" instead.
Just create a new project and add some code as in attached images. Finally click the "debug" button to program the board via HIWAVE debugger(ICD12 w/ P&E BDM Multilink)
I have some screen shots or you can see the quick start manual.
Ron