Cannot download android image to iMX8 QuadXPlus board with UUU.exe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot download android image to iMX8 QuadXPlus board with UUU.exe

Jump to solution
2,127 Views
mt_android
Contributor I

Hi,

I'm trying to download the pre-built image to iMX8 QuadXPlus MEK board, but it failed. Here is the steps:

a) Change the boot mode switch to 1000 for serial mode.

b) Download "automotive-11.0.0_1.1.0_image_8qmek" pre-built image, and UUU.exe (version 1.3.124)

c) Connect the USB cable to the board, and run the following command:

uuu_imx_android_flash.bat -f imx8qm -e

 

After that, I got an error below:

Success 0 Failure 1


2:1 1/ 1 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f u-boot-imx8qm-mek-uuu.imx.link

 

I'm not sure what the problem is, can anyone help me with this issue?

Thanks a lot.

 

0 Kudos
1 Solution
2,085 Views
joanxie
NXP TechSupport
NXP TechSupport

I tested successfully

joanxie_0-1620639607348.png

check your PC recognize your board or not, and check the log file from uart port

View solution in original post

0 Kudos
3 Replies
2,082 Views
joanxie
NXP TechSupport
NXP TechSupport

I tested imx8qm, if you use imx8qxp, pls tell me what version you use? B0 or C0?

0 Kudos
2,086 Views
joanxie
NXP TechSupport
NXP TechSupport

I tested successfully

joanxie_0-1620639607348.png

check your PC recognize your board or not, and check the log file from uart port

0 Kudos
2,078 Views
mt_android
Contributor I

Hi,

Now, I am using iMX8 QuadMax board now, instead of QuadXPlus. And it works. Thank you for your reply.

0 Kudos