Hi,
I submitted it to i.MX Processors, but I will submit it again in the solution because it includes the contents of the config tool.
I set the pin layout with the setting tool.
After setting UART communication TX and RX, I set CTS and RTS.
The error red did not occur when setting CTS and RTS.
Swapping RTS and CTS with the tool did not result in an error.
The RX and TX were able to communicate on the board, but the RTS and CTS signals collided.
(1) Why didn't the tool generate an error?
(2) Can I change only RTS and CTS like a tool?
(3) Does the tool consider DCE / DTE registers?
(4) Is there a register that can invalidate the DCE / DTE register?
・TOOL
Cofig Tools for i.MX6 Version 9.0
・DEVICE
MCIMX6Y2CVM08AV
best regard.