lpspi reading jedecID from flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpspi reading jedecID from flash

Jump to solution
1,498 Views
adi2Intel
Contributor III

Hello

on the 105x

trying to use lpspi interface to initiate spi transactions

I am using the SDK example: lpspi_btb_interrupt_master

I am connected to an external board with the flash

trying to read the JEDEC ID with opcode 0x9F according to windbond spec:

adi2Intel_0-1684929915745.png

 

but I dont receive any data on the MISO line:

adi2Intel_1-1684929967639.png

or with the lpspi poliing example:

adi2Intel_0-1684932523986.png

 

 

when using the FLEX_SPI interface, with SDK example "nor_polling_transfer" ,no problems:

adi2Intel_3-1684930025674.png

 

what could be the issue?

maybe these examples lpspi_btb_interrupt_master and lpspi_btb_polling_master are not fit to this kind of task? maybe they are BTB dedicated?

 

thanks

 

Labels (1)
0 Kudos
Reply
1 Solution
1,357 Views
adi2Intel
Contributor III

the issue was some hardware issues

example reading jedec code:

 

    /*Master config*/
    LPSPI_MasterGetDefaultConfig(&masterConfig);
    masterConfig.baudRate = TRANSFER_BAUDRATE;
    masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;

    srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
    LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);
    uint32_t jedecId;
    uint8_t readdata;
        PRINTF("READ JEDEC");
        jedecId = 0;
        masterTxData[0] = 0x9F;
        masterTxData[1] = 0xFF;
        masterTxData[2] = 0xFF;
        masterTxData[3] = 0xFF;
        masterTxData[4] = 0xFF;
        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = masterTxData;
        masterXfer.rxData   = &jedecId;
        masterXfer.dataSize = 4;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);

 

example for reading and programming page in 4 byte mode (32 bit address, after sending 0xB7 opcode):

PRINTF("READ ADDRESS 0X0");
        uint8_t page[262];
        masterTxData[0] = 0x0B;
        masterTxData[1] = 0x0;
        masterTxData[2] = 0x0;
        masterTxData[3] = 0x0;
        masterTxData[4] = 0x0;
        masterTxData[5] = 0xFF;	//DUMMY BYTE

        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = masterTxData;
        masterXfer.rxData   = page;
        masterXfer.dataSize = 262;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_SetDummyData(EXAMPLE_LPSPI_MASTER_BASEADDR, 0xFF); // Set dummy data to 0xFF

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);


        PRINTF("WR EN");
		masterTxData[0] = 0x06;

		/*Start master transfer, transfer data to slave.*/
		masterXfer.txData   = masterTxData;
		masterXfer.rxData   = NULL;
		masterXfer.dataSize = 1;
		masterXfer.configFlags =
			EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

		LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);


		PRINTF("PROGRAM ADDRESS 0X0");
        uint8_t progpage[267];
        int i;
        for( i=5;i<267;i++)
        {
        	progpage[i] = i - 5;
        }
        progpage[0] = 0x02;
        progpage[1] = 0x0;
        progpage[2] = 0x0;
        progpage[3] = 0x0;
        progpage[4] = 0x0;
        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = progpage;
        masterXfer.rxData   = NULL;
        masterXfer.dataSize = 262;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);

 

 

View solution in original post

0 Kudos
Reply
5 Replies
1,358 Views
adi2Intel
Contributor III

the issue was some hardware issues

example reading jedec code:

 

    /*Master config*/
    LPSPI_MasterGetDefaultConfig(&masterConfig);
    masterConfig.baudRate = TRANSFER_BAUDRATE;
    masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;

    srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
    LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);
    uint32_t jedecId;
    uint8_t readdata;
        PRINTF("READ JEDEC");
        jedecId = 0;
        masterTxData[0] = 0x9F;
        masterTxData[1] = 0xFF;
        masterTxData[2] = 0xFF;
        masterTxData[3] = 0xFF;
        masterTxData[4] = 0xFF;
        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = masterTxData;
        masterXfer.rxData   = &jedecId;
        masterXfer.dataSize = 4;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);

 

example for reading and programming page in 4 byte mode (32 bit address, after sending 0xB7 opcode):

PRINTF("READ ADDRESS 0X0");
        uint8_t page[262];
        masterTxData[0] = 0x0B;
        masterTxData[1] = 0x0;
        masterTxData[2] = 0x0;
        masterTxData[3] = 0x0;
        masterTxData[4] = 0x0;
        masterTxData[5] = 0xFF;	//DUMMY BYTE

        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = masterTxData;
        masterXfer.rxData   = page;
        masterXfer.dataSize = 262;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_SetDummyData(EXAMPLE_LPSPI_MASTER_BASEADDR, 0xFF); // Set dummy data to 0xFF

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);


        PRINTF("WR EN");
		masterTxData[0] = 0x06;

		/*Start master transfer, transfer data to slave.*/
		masterXfer.txData   = masterTxData;
		masterXfer.rxData   = NULL;
		masterXfer.dataSize = 1;
		masterXfer.configFlags =
			EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

		LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);


		PRINTF("PROGRAM ADDRESS 0X0");
        uint8_t progpage[267];
        int i;
        for( i=5;i<267;i++)
        {
        	progpage[i] = i - 5;
        }
        progpage[0] = 0x02;
        progpage[1] = 0x0;
        progpage[2] = 0x0;
        progpage[3] = 0x0;
        progpage[4] = 0x0;
        /*Start master transfer, transfer data to slave.*/
        masterXfer.txData   = progpage;
        masterXfer.rxData   = NULL;
        masterXfer.dataSize = 262;
        masterXfer.configFlags =
            EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;

        LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);

 

 

0 Kudos
Reply
1,473 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @adi2Intel,

The LPSPI and FlexSPI modules are inheritably different. As stated by my colleague on the following community post: "the FlexSPI module is dedicated to communicate with Flash-like serial devices. It has a set of dedicated features (like LUT command sequences) for such type of accesses. For SPI communication with a "generic" (non-Flash) SPI devices, the LPSPI module should be used."

As you mention, the BTB examples are meant to show a generic SPI communication between two boards. If you are looking for a standard SPI communication example (not between two boards) refer to the "lpspi_interrupt" example.

BR,
Edwin.

0 Kudos
Reply
1,449 Views
adi2Intel
Contributor III

Can we use the LPSPI  to read and write a flash device device using single SPI protocol?

or even use the LPSPI to read JEDEC ID?

basically our device using the flexSPI port to  read and write another flash device , and our device has 4 LPSPI ports .

 

 

0 Kudos
Reply
1,430 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @adi2Intel,

From the W25Q32JV Datasheet: "The W25Q32JV supports the standard Serial Peripheral Interface (SPI)", so it is possible. As mentioned on your previous post, a good example to refer to for LPSPI read/write with NOR Flash would be the "flashloader" example under "bootloader_examples". With the right modifications to the LUT table, you should be able to communicate with the NOR Flash without issues.

BR
Edwin.

0 Kudos
Reply
1,360 Views
adi2Intel
Contributor III

Hi Edwin

I was able to communicate with the FLASH device using the example for the "lpspi_polling_master"

it was an issue of voltages and power.

example for reading status register:

adi2Intel_0-1685519972262.png

 

 

0 Kudos
Reply