i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

ソリューションへジャンプ
1,280件の閲覧回数
WJC
Contributor I

Hello,

I want to use the Gigabit Ethernet to do MAC to MAC without PHY (RGMII to RGMII) on RT1170.
Does this work?

 

0 件の賞賛
1 解決策
1,204件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,220件の閲覧回数
WJC
Contributor I


ENET 10/100Mbps can use MAC-to-MAC without phy.

Attached the simple block diagram.

Thanks in advance.

WJC

0 件の賞賛
1,205件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

0 件の賞賛
1,197件の閲覧回数
WJC
Contributor I

Thanks for your reply.

0 件の賞賛
1,249件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

@WJC 

 

RT1170 does not support MAC TO MAC connection without PHY.  Because RT1170 doesn't have delay line inserted on rx/tx data sampling capturing path, so timing will not match.

 

Regards

Daniel