The SLN-VIZN-IOT doesn't have parallel LCD port or MSI port
The user guide says mus be "Riverdi Display"
I assume any with usb controller must work?
Resolution, size, controller, etc?
Thanks in advance.
Hi Oscar,
I have received feedback from internal team:
customer can use USB-SPI bridge board with any SPI display with Video over USB support but it also depends on additional control signals like Reset, Chip-Select, Enable, etc.
Best regards,
Felipe
Hi Oscar,
I asked this question to applications engineering team and I have received the following feedback.
there is SPI FT801 controller on RVT28AEFNWC00. From my practical experience I can recommend displays which are using controller from Solomon Systech like SSD1963 or Ilitek ILI9341.
There are many variants of LCDs using these controllers.
I hope this helps.
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------
Hi Felipe:
Unfortunately the indicated models do not have video over USB, the
manual.
Obviously with SPI I can integrate the video but it involves
development and we want a quick integration.
In the user manual it says on page 23 "Configures the display
output device to use either video over USB or the Riverdi display
/Requires Riverdi display/"_/*
/__//__/
/__/*/_ In Riverdi there's a Hermes Board-SPI USB bridge board.
Do I need to buy this plus the display shown in the email or any
other display?
Thanks in advance.
El 27/05/2020 a las 10:44 a. m., nxf46115 escribió:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: Wich model of Riverdi Display at SLN-VIZN-IOT?
reply from Felipe García
<https://community.nxp.com/people/nxf46115?et=watches.email.thread> in
/i.MX RT/ - View the full discussion
<https://community.nxp.com/message/1318174?commentID=1318174&et=watches.email.thread#comment-1318174>
>
Hi Jive
At SPF-SOL0005_C.pdf page 8 has a display interface conector. (in a
SLN-VIZN-IOT-DESIGN-FILES)
J32 seems to me an SPI port, many Riverdi displays have an SPI port.
I think is that I need!?
About the theme of type touch, I guess don't care?
Thanks in advance.
Oscar
El 05/06/2020 a las 05:25 p. m., nxf46115 escribió:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: Wich model of Riverdi Display at SLN-VIZN-IOT?
reply from Felipe García
<https://community.nxp.com/people/nxf46115?et=watches.email.thread> in
/i.MX RT/ - View the full discussion
<https://community.nxp.com/message/1322815?commentID=1322815&et=watches.email.thread#comment-1322815>
>