Wich model of Riverdi Display at SLN-VIZN-IOT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wich model of Riverdi Display at SLN-VIZN-IOT?

1,520 Views
odelmote
Contributor II

The SLN-VIZN-IOT doesn't have parallel LCD port or MSI port

The user guide says mus be "Riverdi Display"

I assume any with usb controller must work?

Resolution, size, controller, etc?

Thanks in advance.

Labels (1)
0 Kudos
5 Replies

1,339 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Oscar,

 

I have received feedback from internal team:

 

customer can use USB-SPI bridge board with any SPI display with Video over USB support but it also depends on additional control signals like Reset, Chip-Select, Enable, etc.

 

Best regards,

Felipe

0 Kudos

1,339 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Oscar,

 

I asked this question to applications engineering team and I have received the following feedback.

there is SPI FT801 controller on RVT28AEFNWC00. From my practical experience I can recommend displays which are using controller from Solomon Systech like SSD1963 or Ilitek ILI9341.

 

There are many variants of LCDs using these controllers.

I hope this helps.

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------

0 Kudos

1,339 Views
odelmote
Contributor II

Hi Felipe:

    Unfortunately the indicated models do not have video over USB, the

manual.

    Obviously with SPI I can integrate the video but it involves

development and we want a quick integration.

    In the user manual it says on page 23 "Configures the display

output device to use either video over USB or the Riverdi display

/Requires Riverdi display/"_/*

/__//__/

/__/*/_    In Riverdi there's a Hermes Board-SPI USB bridge board.

    Do I need to buy this plus the display shown in the email or any

other display?

Thanks in advance.

El 27/05/2020 a las 10:44 a. m., nxf46115 escribió:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Wich model of Riverdi Display at SLN-VIZN-IOT?

reply from Felipe García

<https://community.nxp.com/people/nxf46115?et=watches.email.thread> in

/i.MX RT/ - View the full discussion

<https://community.nxp.com/message/1318174?commentID=1318174&et=watches.email.thread#comment-1318174>

>

0 Kudos

1,339 Views
FelipeGarcia
NXP Employee
NXP Employee

I am checking this internally. Any update I will let you know.

 

Best regards,

Felipe

0 Kudos

1,339 Views
odelmote
Contributor II

Hi Jive

    At SPF-SOL0005_C.pdf page 8 has a display interface conector. (in a

SLN-VIZN-IOT-DESIGN-FILES)

    J32 seems to me an SPI port, many Riverdi displays have an SPI port.

    I think is that I need!?

    About the theme of type touch, I guess don't care?

Thanks in advance.

Oscar

El 05/06/2020 a las 05:25 p. m., nxf46115 escribió:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Wich model of Riverdi Display at SLN-VIZN-IOT?

reply from Felipe García

<https://community.nxp.com/people/nxf46115?et=watches.email.thread> in

/i.MX RT/ - View the full discussion

<https://community.nxp.com/message/1322815?commentID=1322815&et=watches.email.thread#comment-1322815>

>

0 Kudos