TCM & Cache...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TCM & Cache...

Jump to solution
1,099 Views
EdSutter
Senior Contributor II

I'm working on a new feature (SPEEX echo cancellation) for my hardware that, as of right now, is not working because of what appears to be not-enough-horsepower in the '1062.  Its still pretty early, so its possible (i.e. likely) I just have a problem with how I'm using the echo canceller, but it raises a general question that I'm sure has already been answered somewhere regarding optimization...

I have text and data mapped to ITCM and DTCM respectively, so does it matter how I have cache configured (MPU) for those areas? Is cache even in the picture when using TCM?  

tx

Ed

0 Kudos
Reply
1 Solution
1,094 Views
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

View solution in original post

0 Kudos
Reply
2 Replies
1,089 Views
EdSutter
Senior Contributor II

That's what I thought...

Thanks Mark

0 Kudos
Reply
1,095 Views
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

0 Kudos
Reply