Query related to Power consumption is DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Query related to Power consumption is DMA

跳至解决方案
1,011 次查看
suhel_mulla
Contributor III

Hello,

We are using NXP i.MX RT 1052 controller.

We already know that DMA is used for parallel processing and to improve overall processor performance.

But, we are trying to understand whether DMA can be used to minimize current consumption or not.

My question is as below -

Consider the below 2 cases,

  1. SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
  2. Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using CPU.

For these 2 cases, in which case, the current consumption will be more?

Also, please provide if any analytical document is available for this.

标签 (1)
标记 (5)
0 项奖励
1 解答
1,006 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) My question is as below -
Consider the below 2 cases,
SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using the CPU.
For these 2 cases, in which case, the current consumption will be more?
-- Case 2 will cost more power consumption.
And there's an article that explains the DMA's advantage and hopes it can help you.

Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
3 回复数
1,001 次查看
suhel_mulla
Contributor III

Thanks for the answer and sharing the article. It will solve my query.

0 项奖励
1,005 次查看
suhel_mulla
Contributor III

Thanks for the answer.

Can you share link of the article which explains it?

0 项奖励
1,007 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) My question is as below -
Consider the below 2 cases,
SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using the CPU.
For these 2 cases, in which case, the current consumption will be more?
-- Case 2 will cost more power consumption.
And there's an article that explains the DMA's advantage and hopes it can help you.

Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励