Is it correct that the maximum supply voltage for DCDC_IN on the RT1062 (silicon A0) is 3.0V and not 3.6V ?
Its not mentioned in the datasheet or errata, but only in the Hardware Development Guide
So far everything seems to work without the magic smoke coming out :smileywink:
Running at 3.3V.
First program running, board is designed for testing of RT1064 which is not quite available yet, I mounted a RT1062 instead and made it possible to connect a Quad SPI Flash (at 0x60000000) to start testing.
Once I know this is 100% working as it should I will be able to save the CPU/SDRAM design/layout and use this in the subsequent "real projects".
Thanks for help so far :smileyhappy:
Board is a 4 layer 0.8 mm thick from JLCPCB (US$ 79,- incl DHL shipping. 8 days from gerber to PCB arrived at doorstep).
Hi Carsten
Hardware Development Guide gives references to silicon A0&3.0V
for i.MXRT1050, so seems this is not true for RT1062.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor,
so there is nothing that points to that the RT1062 (and RT1064) should not be able to use 3.3V for A0 silicon ?
The hardware development guide I mentioned is for both RT1050 and RT1060:
I will know in a week or so when PCB arrives here, then I will see what happens (I have the possibility to change LDO so I can use either 3.0 or 3.3V)