Connecting a RK055HDMIPI4M TFT display to a i.MXRT1170-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting a RK055HDMIPI4M TFT display to a i.MXRT1170-EVK

Jump to solution
1,201 Views
skruglewicz
Contributor III

I have a i.MXRX1170-EVK that has RK055HDMIPI4M TFT display included. Does anyone know how to connect the ribbon cable from the TFT Display board to the .iMXRT1170-EVK MIPI LCD connector?

More specifically, the orientation of the connector?

The TFT Ribbon cable has a blue tab on one side?

I cannot seem to find any installation instructions on this site?

Any help would be greatly appreciated.

Thanks in Advance.

Steve K

 

0 Kudos
1 Solution
1,169 Views
skruglewicz
Contributor III

Thank you

I just ordered the part from mouser.com. should be here in a couple of days

View solution in original post

0 Kudos
4 Replies
1,197 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Steve,

Please go through form pic1 to pic3.

pic1, pull out black part.

jingpan_0-1622448622136.png

pic2, insert the cable.

jingpan_1-1622448685714.png

Pic3, plug the black part.

jingpan_3-1622448745977.png

 

Regards,

Jing

0 Kudos
1,190 Views
skruglewicz
Contributor III

hi Jing,

Thanks so much for your help. I understand now how to install the ribbon cable.

I sort of have an issue with the BLACK Part though. When I tried to remove it I broke of one of the end.

The cable still seems to hold fast but, I was wondering if there is a part number for the black part or the entire connector? I could order it online.

Thanks again for your help

 

broken black partbroken black part

0 Kudos
1,185 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

here is a BOM table in RT1170 EVK design package. It shows this is "CON 1X40 FPC SMT RA 0.5MM 89H AU". Manufactured by WURTH ELEKTRONIK EISOS GMBH & CO. KG (ELECTRONIC & ELECTROMEHANICAL COMP). Mfg part number is 68714014022.

 

Regards

0 Kudos
1,170 Views
skruglewicz
Contributor III

Thank you

I just ordered the part from mouser.com. should be here in a couple of days

0 Kudos