Hi,
can anyone suggest a camera module for RT1050 EVKB which is actively Available with a maximum length of cable.
Regards,
Jagadeesh s
Hi Jagadeesh,
We can suggest MT9M114 module that is the one we use in our SDK examples.
https://www.nxp.com/docs/en/application-note/AN12110.pdf
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------
Hi,
What is the Maximum length of the cable between camera module and the evaluation Board RT1050.
Please provide us the link to buy online.
Best Regards,
jagadeesh