Connect Camera to i.MX RT685 EVK for Computer Vision Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connect Camera to i.MX RT685 EVK for Computer Vision Application

908 次查看
mgandhi
Contributor II

I'm interested in prototyping a computer vision application on the RT685 EVK.  I plan on using the eIQ Glow toolchain to run a computer vision model.  Since the EVK doesn't come with a camera or camera connector, is there a recommended way to connect a camera?

标签 (1)
0 项奖励
3 回复数

894 次查看
mgandhi
Contributor II

Ok. Thanks.  Does NXP have any recommendations for a camera?  Are there any documented integrations with a I2C or SPI camera?  Perhaps an application note or blog.  If NXP doesn't have anything perhaps a community effort or blog.  This will help me get started.  

Given the performance numbers that NXP is promoting during its webinars covering the GLOW AI model compiler, it would be really helpful to have a starting point for integrating a camera with the board. 

Appreciate the help!  

0 项奖励

883 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Not a problem. First I'd recommend to check the advantages that you might have in using the RT106x family that also supports the eIQ Glow. Here you have the parallel camera sensor interface and the camera we use is the MT9M114. Here is an application note for reference:

Developing a Camera Application with i.MX

AN12110Software.zip

 

For the i.MXRT 6xx family there are no examples using an alternative camera interface such as I2C or SPI. This implementation will have to be custom for your application.

 

Best Regards,

Sabina

0 项奖励

896 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

The RT6xx family does not have multimedia connectivity for a camera interface as other RT families such as the RT106x. 

If you would like to continue to work with the RT6xx then I'd recommend to choose a camera that is capable of communication via I2C, SPI, etc.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励