i.MX RT知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT Knowledge Base

标签

讨论

排序依据:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/t5/i-MX-Community-Articles/Effortless-GUI-Development-with-NXP-Microcontrollers/ba-p/1131179  
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345190  
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/t5/eIQ-Machine-Learning-Software/eIQ-on-i-MX-RT1064-EVK/ta-p/1123602 
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1050-HAB-Encrypted-Image-Generation-and-Analysis/ta-p/1124877  
查看全文
In the tutorial, I'd like to show the steps of deploying an image classification model on i.MX RT1060 to enabling you to classify fashion images and categories. In the first part of this tutorial, we will review the Fashion MNIST dataset, including how to download it to your system. From there we’ll define a simple CNN network using the TensorFlow platform. Next, we’ll train our CNN model on the Fashion MNIST dataset, train it, and review the results. Finally, we'll optimize the model, after that, the model will be smaller and increase inferencing speed, which is valuable for source-limited devices such as MCU. Let’s go ahead and get started! Fashion MNIST dataset The Fashion MNIST dataset was created by the e-commerce company, Zalando. Fig 1 Fashion MNIST dataset As they note on their official GitHub repo for the Fashion MNIST dataset, there are a few problems with the standard MNIST digit recognition dataset: It’s far too easy for standard machine learning algorithms to obtain 97%+ accuracy. It’s even easier for deep learning models to achieve 99%+ accuracy. The dataset is overused. MNIST cannot represent modern computer vision tasks. Zalando, therefore, created the Fashion MNIST dataset as a drop-in replacement for MNIST. 60,000 training examples 10,000 testing examples 10 classes: T-shirt/top, Trouser, Pullover, Dress, Coat, Sandal, Shirt, Sneaker, Bag, Ankle boot 28×28 grayscale images The code below loads the Fashion-MNIST dataset using the TensorFlow and creates a plot of the first 25 images in the training dataset. import tensorflow as tf import numpy as np # For easy reset of notebook state. tf.keras.backend.clear_session() # load dataset fashion_mnist = tf.keras.datasets.fashion_mnist (train_images, train_labels), (test_images, test_labels) = fashion_mnist.load_data() lass_names = ['T-shirt/top', 'Trouser', 'Pullover', 'Dress', 'Coat', 'Sandal', 'Shirt', 'Sneaker', 'Bag', 'Ankle boot'] plt.figure(figsize=(8,8)) for i in range(25): plt.subplot(5,5,i+1,) plt.tight_layout() plt.imshow(train_images[i]) plt.xlabel(lass_names[train_labels[i]]) plt.xticks([]) plt.yticks([]) plt.grid(False) plt.show() Fig 2 Running the code loads the Fashion-MNIST train and test dataset and prints their shape. Fig 3 We can see that there are 60,000 examples in the training dataset and 10,000 in the test dataset and that images are indeed square with 28×28 pixels. Creating model We need to define a neural network model for the image classify purpose, and the model should have two main parts: the feature extraction and the classifier that makes a prediction. Defining a simple Convolutional Neural Network (CNN) For the convolutional front-end, we build 3 layers of convolution layer with a small filter size (3,3) and a modest number of filters followed by a max-pooling layer. The last filter map is flattened to provide features to the classifier. As we know, it's a multi-class classification task, so we will require an output layer with 10 nodes in order to predict the probability distribution of an image belonging to each of the 10 classes. In this case, we will require the use of a softmax activation function. And between the feature extractor and the output layer, we can add a dense layer to interpret the features. All layers will use the ReLU activation function and the He weight initialization scheme, both best practices. We will use the Adam optimizer to optimize the sparse_categorical_crossentropy loss function, suitable for multi-class classification, and we will monitor the classification accuracy metric, which is appropriate given we have the same number of examples in each of the 10 classes. The below code will define and run it will show the struct of the model. # Define a Model model = tf.keras.models.Sequential() # First Convolution ,Kernel:16*3*3 model.add( tf.keras.layers.Conv2D(16, (3, 3), activation='relu', kernel_initializer='he_uniform',input_shape=(28, 28, 1))) model.add( tf.keras.layers.MaxPooling2D((2, 2))) # Second Convolution ,Kernel:32*3*3 model.add( tf.keras.layers.Conv2D(32, (3, 3), activation='relu',kernel_initializer='he_uniform')) model.add( tf.keras.layers.MaxPooling2D((2, 2))) # Third Convolution ,Kernel:32*3*3 model.add( tf.keras.layers.Conv2D(32, (3, 3), activation='relu',kernel_initializer='he_uniform')) model.add( tf.keras.layers.Flatten()) model.add( tf.keras.layers.Dense(32, activation='relu',kernel_initializer='he_uniform')) model.add( tf.keras.layers.Dense(10, activation='softmax')) Fig 4 Training Model After the model is defined, we need to train it. The model will be trained using 5-fold cross-validation. The value of k=5 was chosen to provide a baseline for both repeated evaluation and to not be too large as to require a long running time. Each validation set will be 20% of the training dataset or about 12,000 examples. The training dataset is shuffled prior to being split and the sample shuffling is performed each time so that any model we train will have the same train and validation datasets in each fold, providing an apples-to-apples comparison. We will train the baseline model for a modest 20 training epochs with a default batch size of 32 examples. The validation set for each fold will be used to validate the model during each epoch of the training run, so we can later create learning curves, and at the end of the run, we use the test dataset to estimate the performance of the model. As such, we will keep track of the resulting history from each run, as well as the classification accuracy of the fold. The train_model() function below implements these behaviors, taking the training dataset and test dataset as arguments, and returning a list of accuracy scores and training histories that can be later summarized. from sklearn.model_selection import KFold # train a model using k-fold cross-validation def train_model(dataX, dataY, n_folds=5): scores, histories = list(), list() # prepare cross validation kfold = KFold(n_folds, shuffle=True, random_state=1) for train_ix, validate_ix in kfold.split(dataX): # select rows for train and test trainX, trainY, validate_X, validate_Y = dataX[train_ix], dataY[train_ix], dataX[validate_ix], dataY[validate_ix] # fit model history = model.fit(trainX, trainY, epochs=20, batch_size=32, validation_data=(validate_X, validate_Y), verbose=0) # evaluate model _, acc = model.evaluate(validate_X, validate_Y, verbose=0) print("Accurary: {:.4f},Total number of figures is {:0>2d}".format(acc * 100.0, len(testY))) # append scores scores.append(acc) histories.append(history) return scores, histories Module Summary After the model has been trained, we can present the results. There are two key aspects to present: the diagnostics of the learning behavior of the model during training and the estimation of the model performance. These can be implemented using separate functions. First, the diagnostics involve creating a line plot showing model performance on the train and validate set during each fold of the k-fold cross-validation. These plots are valuable for getting an idea of whether a model is overfitting, underfitting, or has a good fit for the dataset. We will create a single figure with two subplots, one for loss and one for accuracy. Blue lines will indicate model performance on the training dataset and orange lines will indicate performance on the hold-out validate dataset. The summarize_diagnostics() function below creates and shows this plot given the collected training histories. # plot diagnostic learning curves def summarize_diagnostics(histories): for i in range(len(histories)): # plot loss plt.subplot(2,1,1) plt.title('Cross Entropy Loss') plt.plot(histories[i].history['loss'], color='blue', label='train') plt.plot(histories[i].history['val_loss'], color='orange', label='test') # plot accuracy plt.subplot(2,1,2) plt.title('Classification Accuracy') plt.plot(histories[i].history['accuracy'], color='blue', label='train') plt.plot(histories[i].history['val_accuracy'], color='orange', label='test') plt.show() Fig 5 Next, the classification accuracy scores collected during each fold can be summarized by calculating the mean and standard deviation. This provides an estimate of the average expected performance of the model trained on the test dataset, with an estimate of the average variance in the mean. We will also summarize the distribution of scores by creating and showing a box and whisker plot. The summarize_performance() function below implements this for a given list of scores collected during model training. # summarize model performance def summarize_performance(scores): # print summary print('Accuracy: mean={:.4f} std={:.4f}, n={:0>2d}'.format(np.mean(trained_scores)*100, np.std(trained_scores)*100, len(scores))) # box and whisker plots of results plt.boxplot(scores) plt.show()   Fig 6 Verifying predictions According to the above figure, we see that the final trained model can get up to around 87.6% accuracy when predicting the test dataset. And with the trained model, running the below code will demonstrate the result of predictions about some images. def plot_image(i, predictions_array, true_label, img): true_label, img = true_label[i], img[i] plt.grid(False) plt.xticks([]) plt.yticks([]) plt.imshow(img.reshape(28, 28), cmap=plt.cm.binary) predicted_label = np.argmax(predictions_array) if predicted_label == true_label: color = 'blue' else: color = 'red' plt.xlabel("{} {:2.0f}% ({})".format(class_names[predicted_label], 100*np.max(predictions_array), class_names[true_label]), color=color) def plot_value_array(i, predictions_array, true_label): true_label = true_label[i] plt.grid(False) plt.xticks(range(10)) plt.yticks([]) thisplot = plt.bar(range(10), predictions_array, color="#777777") plt.ylim([0, 1]) predicted_label = np.argmax(predictions_array) thisplot[predicted_label].set_color('red') thisplot[true_label].set_color('blue') predictions = model.predict(test_images) # Plot the first X test images, their predicted labels, and the true labels. # Color correct predictions in blue and incorrect predictions in red. num_rows = 5 num_cols = 3 num_images = num_rows*num_cols plt.figure(figsize=(2*2*num_cols, 2*num_rows)) for i in range(num_images): plt.subplot(num_rows, 2*num_cols, 2*i+1) plot_image(i, predictions[i], test_labels, test_images) plt.subplot(num_rows, 2*num_cols, 2*i+2) plot_value_array(i, predictions[i], test_labels) plt.tight_layout() plt.show()   Fig 7 Model quantization Post-training quantization is a conversion technique that can reduce model size while also improving CPU and hardware accelerator latency, with little degradation in model accuracy, especially it's crucial to embedded platforms, as it lacks the compute-intensive performance, the Flash and RAM memory is also very limited. TensorFlow Lite is able to be used to convert an already-trained float TensorFlow model to the TensorFlow Lite format. In addition, the TensorFlow Lite provides several approaches to optimize the mode, among these ways, Integer quantization is an optimization strategy that converts 32-bit floating-point numbers (such as weights and activation outputs) to the nearest 8-bit fixed-point numbers. This results in a smaller model and increased inferencing speed, which is very valuable for low-power devices such as microcontrollers. The below codes show how to implement the Integer quantization of the trained model, and after running these codes, we can find that the size of Tensorflow Lite mode reduces almost 64.9 KB versus the original model, becomes about 32% of the original size(Fig 8). import os # Convert using integer-only quantization def representative_data_gen(): for input_value in tf.data.Dataset.from_tensor_slices(tf.cast(train_images,tf.float32)).shuffle(500).batch(1).take(150): yield [input_value] # Convert using dynamic range quantization converter = tf.lite.TFLiteConverter.from_keras_model(model) converter.optimizations = [tf.lite.Optimize.DEFAULT] tflite_model_quant = converter.convert() # Save the model to disk open("model_dynamic_range_quantization.tflite", "wb").write(tflite_model_quant) ## Size difference Dynamic_range_quantization_model_size = os.path.getsize("model_dynamic_range_quantization.tflite") print("Dynamic range quantization model is %d bytes" % Dynamic_range_quantization_model_size) converter = tf.lite.TFLiteConverter.from_keras_model(model) converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.representative_dataset = representative_data_gen # Ensure that if any ops can't be quantized, the converter throws an error converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8] # Set the input and output tensors to uint8 (APIs added in r2.3) converter.inference_input_type = tf.uint8 converter.inference_output_type = tf.uint8 tflite_model_advanced_quant = converter.convert() # Save the model to disk open("model_integer_only_quantization.tflite", "wb").write(tflite_model_advanced_quant) Integer_only_quantization_model_size = os.path.getsize("model_integer_only_quantization.tflite") print("Integer_only_quantization_model is %d bytes" % Integer_only_quantization_model_size) difference = Dynamic_range_quantization_model_size - Integer_only_quantization_model_size print("Difference is %d bytes" % difference) Fig 8 Evaluating the TensorFlow Lite model Now we'll run inferences using the TensorFlow Lite Interpreter to compare the model accuracies. First, we need a function that runs inference with a given model and images, and then returns the predictions: # Helper function to run inference on a TFLite model def run_tflite_model(tflite_file, test_image_indices): # Initialize the interpreter interpreter = tf.lite.Interpreter(model_path=str(tflite_file)) interpreter.allocate_tensors() input_details = interpreter.get_input_details()[0] output_details = interpreter.get_output_details()[0] predictions = np.zeros((len(test_image_indices),), dtype=int) for i, test_image_index in enumerate(test_image_indices): test_image = test_images[test_image_index] test_label = test_labels[test_image_index] # Check if the input type is quantized, then rescale input data to uint8 if input_details['dtype'] == np.uint8: input_scale, input_zero_point = input_details["quantization"] test_image = test_image / input_scale + input_zero_point test_image = np.expand_dims(test_image, axis=0).astype(input_details["dtype"]) interpreter.set_tensor(input_details["index"], test_image) interpreter.invoke() output = interpreter.get_tensor(output_details["index"])[0] predictions[i] = output.argmax() return predictions Next, we'll compare the performance of the original model and the quantized model on one image. model_basic_quantization.tflite is the original TensorFlow Lite model with floating-point data. model_integer_only_quantization.tflite is the last model we converted using integer-only quantization (it uses uint8 data for input and output). Let's create another function to print our predictions and run it for testing. import matplotlib.pylab as plt # Change this to test a different image test_image_index = 1 ## Helper function to test the models on one image def test_model(tflite_file, test_image_index, model_type): global test_labels predictions = run_tflite_model(tflite_file, [test_image_index]) plt.imshow(test_images[test_image_index].reshape(28,28)) template = model_type + " Model \n True:{true}, Predicted:{predict}" _ = plt.title(template.format(true= str(test_labels[test_image_index]), predict=str(predictions[0]))) plt.grid(False) Fig 9 Fig 10 Then evaluate the quantized model by using all the test images we loaded at the beginning of this tutorial. After summarizing the prediction result of the test dataset, we can see that the prediction accuracy of the quantized model decrease 7% less than the original model, it's not bad. # Helper function to evaluate a TFLite model on all images def evaluate_model(tflite_file, model_type): test_image_indices = range(test_images.shape[0]) predictions = run_tflite_model(tflite_file, test_image_indices) accuracy = (np.sum(test_labels== predictions) * 100) / len(test_images) print('%s model accuracy is %.4f%% (Number of test samples=%d)' % ( model_type, accuracy, len(test_images))) Deploying model Converting TensorFlow Lite model to C file The following code runs xxd on the quantized model, writes the output to a file called model_quantized.cc, in the file, the model is defined as an array of bytes, and prints it to the screen. The output is very long, so we won’t reproduce it all here, but here’s a snippet that includes just the beginning and end. # Save the file as a C source file xxd -i model_integer_only_quantization.tflite > model_quantized.cc # Print the source file cat model_quantized.cc Fig 11 Deploying the C file to project We use the tensorflow_lite_cifar10 demo as a prototype, then replace the original model and do some code modification, below is the code in the modified main file. #include "board.h" #include "fsl_debug_console.h" #include "pin_mux.h" #include "timer.h" #include <iomanip> #include <iostream> #include <string> #include <vector> #include "tensorflow/lite/kernels/register.h" #include "tensorflow/lite/model.h" #include "tensorflow/lite/optional_debug_tools.h" #include "tensorflow/lite/string_util.h" #include "get_top_n.h" #include "model.h" #define LOG(x) std::cout // ---------------------------- Application ----------------------------- // Lenet Mnist model input data size (bytes). #define LENET_MNIST_INPUT_SIZE 28*28*sizeof(char) // Lenet Mnist model number of output classes. #define LENET_MNIST_OUTPUT_CLASS 10 // Allocate buffer for input data. This buffer contains the input image // pre-processed and serialized as text to include here. uint8_t imageData[LENET_MNIST_INPUT_SIZE] = { #include "clothes_select.inc" }; /* Tresholds */ #define DETECTION_TRESHOLD 60 /*! * @brief Initialize parameters for inference * * @param reference to flat buffer * @param reference to interpreter * @param pointer to storing input tensor address * @param verbose mode flag. Set true for verbose mode */ void InferenceInit(std::unique_ptr<tflite::FlatBufferModel> &model, std::unique_ptr<tflite::Interpreter> &interpreter, TfLiteTensor** input_tensor, bool isVerbose) { model = tflite::FlatBufferModel::BuildFromBuffer(Fashion_MNIST_model, Fashion_MNIST_model_len); if (!model) { LOG(FATAL) << "Failed to load model\r\n"; return; } tflite::ops::builtin::BuiltinOpResolver resolver; tflite::InterpreterBuilder(*model, resolver)(&interpreter); if (!interpreter) { LOG(FATAL) << "Failed to construct interpreter\r\n"; return; } int input = interpreter->inputs()[0]; const std::vector<int> inputs = interpreter->inputs(); const std::vector<int> outputs = interpreter->outputs(); if (interpreter->AllocateTensors() != kTfLiteOk) { LOG(FATAL) << "Failed to allocate tensors!"; return; } /* Get input dimension from the input tensor metadata assuming one input only */ *input_tensor = interpreter->tensor(input); auto data_type = (*input_tensor)->type; if (isVerbose) { const std::vector<int> inputs = interpreter->inputs(); const std::vector<int> outputs = interpreter->outputs(); LOG(INFO) << "input: " << inputs[0] << "\r\n"; LOG(INFO) << "number of inputs: " << inputs.size() << "\r\n"; LOG(INFO) << "number of outputs: " << outputs.size() << "\r\n"; LOG(INFO) << "tensors size: " << interpreter->tensors_size() << "\r\n"; LOG(INFO) << "nodes size: " << interpreter->nodes_size() << "\r\n"; LOG(INFO) << "inputs: " << interpreter->inputs().size() << "\r\n"; LOG(INFO) << "input(0) name: " << interpreter->GetInputName(0) << "\r\n"; int t_size = interpreter->tensors_size(); for (int i = 0; i < t_size; i++) { if (interpreter->tensor(i)->name) { LOG(INFO) << i << ": " << interpreter->tensor(i)->name << ", " << interpreter->tensor(i)->bytes << ", " << interpreter->tensor(i)->type << ", " << interpreter->tensor(i)->params.scale << ", " << interpreter->tensor(i)->params.zero_point << "\r\n"; } } LOG(INFO) << "\r\n"; } } /*! * @brief Runs inference input buffer and print result to console * * @param pointer to image data * @param image data length * @param pointer to labels string array * @param reference to flat buffer model * @param reference to interpreter * @param pointer to input tensor */ void RunInference(const uint8_t* image, size_t image_len, const std::string* labels, std::unique_ptr<tflite::FlatBufferModel> &model, std::unique_ptr<tflite::Interpreter> &interpreter, TfLiteTensor* input_tensor) { /* Copy image to tensor. */ memcpy(input_tensor->data.uint8, image, image_len); /* Do inference on static image in first loop. */ auto start = GetTimeInUS(); if (interpreter->Invoke() != kTfLiteOk) { LOG(FATAL) << "Failed to invoke tflite!\r\n"; return; } auto end = GetTimeInUS(); const float threshold = (float)DETECTION_TRESHOLD /100; std::vector<std::pair<float, int>> top_results; int output = interpreter->outputs()[0]; TfLiteTensor *output_tensor = interpreter->tensor(output); TfLiteIntArray* output_dims = output_tensor->dims; // assume output dims to be something like (1, 1, ... , size) auto output_size = output_dims->data[output_dims->size - 1]; /* Find best image candidates. */ GetTopN<uint8_t>(interpreter->typed_output_tensor<uint8_t>(0), output_size, 1, threshold, &top_results, false); if (!top_results.empty()) { auto result = top_results.front(); const float confidence = result.first; const int index = result.second; if (confidence * 100 > DETECTION_TRESHOLD) { LOG(INFO) << "----------------------------------------\r\n"; LOG(INFO) << " Inference time: " << (end - start) / 1000 << " ms\r\n"; LOG(INFO) << " Detected: " << std::setw(10) << labels[index] << " (" << (int)(confidence * 100) << "%)\r\n"; LOG(INFO) << "----------------------------------------\r\n\r\n"; } } } /*! * @brief Main function */ int main(void) { const std::string labels[] = {"T-shirt/top", "Trouser","Pullover", "Dress", "Coat", "Sandal", "Shirt", "Sneaker", "Bag", "Ankle boot"}; /* Init board hardware. */ BOARD_ConfigMPU(); BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); InitTimer(); std::unique_ptr<tflite::FlatBufferModel> model; std::unique_ptr<tflite::Interpreter> interpreter; TfLiteTensor* input_tensor = 0; InferenceInit(model, interpreter, &input_tensor, false); LOG(INFO) << "Fashion MNIST object recognition example using a TensorFlow Lite model.\r\n"; LOG(INFO) << "Detection threshold: " << DETECTION_TRESHOLD << "%\r\n"; /* Run inference on static ship image. */ LOG(INFO) << "\r\nStatic data processing:\r\n"; RunInference((uint8_t*)imageData, (size_t)LENET_MNIST_INPUT_SIZE, labels, model, interpreter, input_tensor); while(1) {} } Testing result After deploying the model in the demo project, then we'll run this demo on the MIMXRT1060 (Fig 12) board for testing. Fig 12 Run the below code to covert the Fashion MNIST image to text The process_image() function can convert a Fashion MNIST image to an include file as static data, then include this file in the demo project. def process_image(image, output_path, num_batch=1): img_data = np.transpose(image, (2, 0, 1)) # Repeat image for batch processing (resulting tensor is NCHW or NHWC) img_data = np.reshape(img_data, (num_batch, img_data.shape[0], img_data.shape[1], img_data.shape[2])) img_data = np.repeat(img_data, num_batch, axis=0) img_data = np.reshape(img_data, (num_batch, img_data.shape[1], img_data.shape[2], img_data.shape[3])) # Serialize image batch img_data_bytes = bytearray(img_data.tobytes(order='C')) image_bytes_per_line = 20 with open(output_path, 'wt') as f: idx = 0 for byte in img_data_bytes: f.write('0X%02X, ' % byte) if idx % image_bytes_per_line == (image_bytes_per_line - 1): f.write('\n') idx = idx + 1 # Return serialized image size return len(img_data_bytes)      2. Run the demo project on board.
查看全文
This document describes the different source clocks and the main modules that manage which clock source is used to derive the system clocks that exists on the i.MX RT’s devices. It’s important to know the different clock sources available on our devices, modifying the default clock configuration may have different purposes since increasing the processor performance, achieving specific baud rates for serial communications, power saving, or simply getting a known base reference for a clock timer. The hardware used for this document is the following: i.MX RT: EVK-MIMXRT1060 Keep in mind that the described hardware and management clock modules in this document are a general overview of the different platforms and the devices listed above are used as a reference example, some terms and hardware modules functionality may vary between devices of the same platform. For more detailed information about the device hardware modules, please refer to your specific device Reference Manual. RT platforms The Clock Controller Module(CCM) facilitates the clock generation in the RT platforms, many clocking variations are possible and the maximum clock frequency for the i.MX RT1060 device is @600MHz.The following image shows a block diagram of the CCM, the three marked sub-modules are important to understand all the clock path from the clock generation(oscillators or crystals) to the clock management for all the peripherals of the board.    Figure 1. Clock Controller Module(CCM) Block Diagram        CCM Analog Submodule This submodule contains all the oscillators and several PLL’s that provide a clock source to the principal CMM module. For example, the i.MX RT1060 device supports 2 internal oscillators that combined with suitable external quartz crystal and external load capacitors provide an accurate clock source, another 2 internal oscillators are available for low power modes and as a backup when the system detects a loss of clock. These oscillators provide a fixed frequency for the several PLL’s inside this module. Internal Clock Sources with external components  Crystal Oscillator @24MHz Many of the serial IO modules depend on the fixed frequency of 24 MHz. The reference clock that generates this crystal oscillator provides an accurate clock source for all the PLL inputs.  Crystal Oscillator @32KHz Generally, RTC oscillators are either implemented with 32 kHz or 32.768 kHz crystals. This Oscillator should always be active when the chip is powered on. Internal Clock sources RC Oscillator @24MHz A lower-power RC oscillator module is available on-chip as a possible alternative to the 24 MHz crystal oscillator after a successful power-up sequence. The 24 MHz RC oscillator is a self-tuning circuit that will output the programmed frequency value by using the RTC clock as its reference. While the power consumption of this RC oscillator is much lower than the 24MHz crystal oscillator, one limitation of this RC oscillator module is that its clock frequency is not as accurate. Oscillator @32KHz The internal oscillator is automatically multiplexed in the clocking system when the system detects a loss of clock. The internal oscillator will provide clocks to the same on-chip modules as the external 32kHz oscillator. Also is used to be useful for quicker startup times and tampering prevention. Note. An external 32KHz clock source must be used since the internal oscillator is not precise enough for long term timekeeping. PLLs There are 7 PLLs in the i.MXRT1060 platform, some with specific functions, for example, create a reference clock for the ARM Core, USB peripherals, etc. Below these PLLs are listed. PLL1 - ARM PLL (functional frequency @600 MHz) PLL2 - System PLL (functional frequency @528 MHz)* PLL3 - USB1 PLL (functional frequency @480 MHz)* PLL4 - Audio PLL PLL5 - Video PLL PLL6 - ENET PLL PLL7 - USB2 PLL (functional frequency @480 MHz) * Two of these PLLs are each equipped with four Phase Fractional Dividers (PFDs) in order to generate additional frequencies for many clock roots.  Each PLLs configuration and control functions like Bypass, Output Enable/Disable, and Power Down modes are accessible individually through its PFDs and global configuration and status registers found at the CCM internal memory registers.        Clock Control Module(CCM) The Clock Control Module (CCM) generates and controls clocks to the various modules in the design and manages low power modes. This module uses the available clock sources(PLL reference clocks and PFDs) to generate the clock roots. There are two important sub-blocks inside the CCM listed below. Clock Switcher This sub-block provides the registers that control which PLLs and PFDs outputs are selected as the reference clock for the Clock Root Generator.  Clock Root Generator This sub-block provides the registers that control most of the secondary clock source programming, including both the primary clock source selection and the clock dividers. The clock roots are each individual clocks to the core, system buses, and all other SoC peripherals, among those, are serial clocks, baud clocks, and special function blocks. All of these clock references are delivered to the Low Power Clock Gating unit(LPCG).        Low Power Clock Gating unit(LPCG) The LPCG block receives the root clocks from CCM and splits them to clock branches for each peripheral. The clock branches are individually gated clocks. The following image shows a detailed block diagram of the CMM with the previously described submodules and how they link together. Figure 2. Clock Management System Example: Configure The ARM Core Clock (PLL1) to a different frequency. The Clock tools available in MCUXpresso IDE, allows you to understand and configure the clock source for the peripherals in the platform. The following diagram shows the default PLL1 mode configured @600MHz, the yellow path shows all the internal modules involved in the clock configuration.  Figure 3. Default PLL configuration after reset. From the previous image notice that PLL1 is attached from the 24MHz oscillator, then the PLL1 is configured with a pre-scaler of 50 to achieve a frequency @1.2GHz, finally, a frequency divider by 2 let a final frequency @600MHz. 1.1 Modify the PLL1 frequency For example, you can use the Clock tools to configure the PLL pre-scaler to 30, select the PLL1 block and then edit the pre-scaler value, therefore, the final clock frequency is @360MHz, these modifications are shown in the following figure.  Figure 4. PLL1 @720MHz, final frequency @360MHz    1.2 Export clock configuration to the project After you complete the clock configuration, the Clock Tool will update the source code in clock_config.c and clock_config.h, including all the clock functional groups that we created with the tool. This will include the clock source for specific peripherals. In the previous example, we configured the PLL1 (ARM PLL) to a functional frequency @360MHz; this is translated to the following structure in source code: “armPllConfig_BOARD_BootClockRUN” and it’s used by “CLOCK_InitArmPll();” inside the “BOARD_BootClockPLL150MRUN();” function.     Figure 5. PLL1 configuration struct  Figure 6. PLL configuration function Example: The next steps describe how to select a clock source for a specific peripheral. 1.1 Configure clock for specific peripheral For example, using the GPT(General Purpose Timer) the available clock sources are the following: Clock Source Off Peripheral Clock High-Frequency Reference Clock Clock Source from an external pin Low-Frequency Reference Clock Crystal Oscillator Figure 7. General Purpose Timer Clocks Diagram Using the available SDK example project “evkmimxrt1060_gpt_timer” a configuration struct for the peripheral “gptConfig” is called from the main initialization function inside the gpt_timer.c source file, the default configuration function with the configuration struct as a parameter, is shown in the following figure. Figure 8. Function that returns a GPT default configuration parameters The function loads several parameters to the configuration struct(gptConfig), one of the fields is the Clock Source configuration, modifying this field will let us select an appropriate clock source for our application, the following figure shows the default configuration parameters inside the “GPT_GetDefaultConfig();” function.  Figure 9. Configuration struct In the default GPT configuration struct, the Peripheral Clock(kGPT_CLockSource_Periph) is selected, the SDK comes with several macros located at “fsl_gpt.h” header file, that helps to select an appropriate clock source. The next figure shows an enumerated type of data that contains the possible clock sources for the GPT.  Figure 10. Available clock sources of the GPT. For example, to select the Low-Frequency Reference Clock the source code looks like the following figure.  Figure 11. Low-Frequency Reference Clock attached to GPT Notice that all the peripherals come with a specific configuration struct and from that struct fields the default clocking parameters can be modified to fit with our timing requirements. 1.2 Modify the Peripheral Clock frequency from Clock Tools One of the GPT clock sources is the “Peripheral Clock Source” this clock line can be modified from the Clock Tools, the following figure shows the default frequency configuration from Clock Tools view. Figure 12. GPT Clock Root inside CMM In the previous figure, the GPT clock line is @75MHz, notice that this is sourced from the primary peripheral clock line that is @600MHz attached to the ARM core clocks. For example, modify the PERCLK_PODF divider selecting it and changing the divider value to 4, the resulting frequency is @37.5Mhz, the following figure illustrates these changes.  Figure 13. GPT & PIT clock line @37.5MHz 1.3 Export clock configuration to the project After you complete the clock configuration, the Clock Tool will update the source code in clock_config.c and clock_config.h, including all the clock functional groups that we created with the tool. This will include the clock source for specific peripherals. In the previous example, we configured the GPT clock root divider by a dividing factor of 4 to achieve a 37.5MHz frequency; this is translated to the following instruction in source code: “CLOCK_SetDiv(kCLOCK_PerclkDiv,3);” inside the “BOARD_BootClockRUN();” function.                Figure 14. Frequency divider function References i.MX RT1060 Processor Reference Manual Also visit LPC's System Clocks  Kinetis System Clocks
查看全文
Introduction A common need for GUI applications is to implement a clock function.  Whether it be to create a clock interface for the end user's benefit, or just to time animations or other actions, implementing an accurate clock is a useful and important feature for GUI applications.  The aim of this document is to help you implement clock functions in your AppWizard project.   Methods When implementing a real-time clock, there are a couple of general methods to do so.   Use an independent timer in your MCU Using animation objects Each of these methods have their advantages and disadvantages.  If you just need a timer that doesn't require extra code and you don't require control or assurance of precision, or maybe you can't spare another timer, using an animation object (method #2) may be a good option in that application.  If your application requires an assurance of precision or requires other real-time actions to be performed that AppWizard can't control, it is best to implement an independent timer in your MCU (method #1).  Method 1:  Independent MCU Timer Implementing a timer via an independent MCU timer allows better control and guarantees the precision because it isn't a shared clock and the developer can adjust the interrupt priorities such that the timer interrupt has the highest priority.  AppWizard timing uses a common timer and then time slices activities similar to how an operating system works.  It is for this reason that implementing an independent MCU timer is best when you need control over the precision of the timer or you need other real-time actions to be triggered by this timer.  When implementing a timer using an independent MCU timer (like the RTC module), an understanding of how to interact with Text widgets is needed. Let's look at this first.   Interacting with Text Widgets Editing Text widgets occurs through the use of the emWin library API (the emWin library is the underlying code that AppWizard builds upon). The Text widget API functions are documented in the emWin Graphic Library User Guide and Reference Manual, UM3001.  Most of the Text widget API functions require a Text widget handle.  Be sure to not confuse this handle for the AppWizard ID.  Imagine a clock example where there are two Text widgets in the interface:  one for the minutes and one for the seconds.  The AppWizard IDs of these objects might be ID_TEXT_MINS and ID_TEXT_SECONDS respectively (again, these are not to be confused with the handle to the Text widget for use by emWin library functions).  The first action software should take is to obtain the handle for the Text widgets.   This can be done using the WM_GetDialogItem function.  The code to get the active window handle and the handle for the two Text widgets is shown below: activeWin = WM_GetActiveWindow(); textBoxMins = WM_GetDialogItem(activeWin, ID_TEXT_MINS); textBoxSecs = WM_GetDialogItem(activeWin, ID_TEXT_SECONDS);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note that this function requires the handle to the parent window of the Text widget.  If your application has multiple windows or screens, you may need to be creative in how you acquire this handle, but for this example, the software can simply call the WM_GetActiveWindow function (since there is only one screen).  When to call these functions can be a bit tricky as well.  They can be called before the MainTask() function of the application is called and the application will not crash.  However, the handles won't be correct and the Text widgets will not be updated as expected.  It's recommended that these handles be initialized when the screen is initialized.  An example of how this would be done is shown below: void cbID_SCREEN_CLOCK(WM_MESSAGE * pMsg) { extern WM_HWIN activeWin; extern WM_HWIN textBoxMins; extern WM_HWIN textBoxSecs; extern WM_HWIN textBoxDbg; if(pMsg->MsgId == WM_INIT_DIALOG) { activeWin = WM_GetActiveWindow(); textBoxMins = WM_GetDialogItem(activeWin, ID_TEXT_MINS); textBoxSecs = WM_GetDialogItem(activeWin, ID_TEXT_SECONDS); textBoxDbg = WM_GetDialogItem(activeWin, ID_TEXT_DBG); } GUI_USE_PARA(pMsg); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Once the Text widget handles have been acquired, the text can be updated using the TEXT_SetText() function or the TEXT_SetDec() function in this case, because the Text widgets are configured for decimal mode, since we want to display numbers.  An example of the code to do this is shown below.  /* TEXT_SetDec(Text Widget Handle, Value as Int, Length, Shift, Sign, Leading Spaces) */ if(TEXT_SetDec(textBoxSecs, (int)gSecs, 2, 0, 0, 0)) { /* Perform action here if necessary */ } if(TEXT_SetDec(textBoxMins, (int)gMins, 2, 0, 0, 0)) { /* Perform action here if necessary */ } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Method 2:  Animation Objects When implementing a real-time clock using animation objects, it is necessary to implement a loop.  This could be done outside of the AppWizard GUI (in your code) but because the timing precision can't be guaranteed, it's just as easy to implement a loop in the AppWizard GUI if you know how (it isn't very intuitive as to how to do this). Before examining the interactions to do this, let's look at the variables and objects needed to do this.  ID_VAR_SECS - This variable holds the current seconds value. ID_VAR_SECS_1 - This variable holds the next second value.  ID_TEXT_SECONDS - Text box that displays the current seconds value. ID_END_CNT - Variable that holds the value at which the seconds rolls over and increments the minute count ID_TEXT_MINS - Text box that holds the current minute count. ID_MIN_END_CNT - Variable that holds the value at which the minutes rolls over (which would also increment the hour count if the hours were implemented). ID_BUTTON_SECS - This is a hidden button that initiates actions when the seconds variable has reached the end count.  Now, here are the interactions used to implement the clock feature using animation interactions.  The heart of the loop are the interactions triggered by ID_VAR_SECS.  ID_VAR_SECS -> ID_VAR_SECS_1:  When ID_VAR_SECS changes, it needs to add one to ID_VAR_SECS_1 so that the animation will animate to one second from the current time. ID_VAR_SECS -> ID_TEXT_SECONDS:  When ID_VAR_SECS changes, it also needs to start the animation from the current value to the next second (ID_VAR_SECS_1). A very essential part of the loop is ensuring the animation restarts every time.  So ID_TEXT_SECONDS needs to change the value of ID_VAR_SECS when the animation ends. ID_VAR_SECS is changed to the current time value, ID_VAR_SECS_1. When the ID_TEXT_SECONDS animation ends, it must also decrement the ID_VAR_END_CNT variable.  This is analogous to the control variable of a "For" loop being updated. This is done using the ADDVALUE job, adding '-1' to the variable, ID_VAR_END_CNT. When ID_VAR_END_CNT changes, it updates the hidden button, ID_BUTTON_SECS, with the new value.  This is analogous to a "For" loop checking whether its control variable is still within its limits.   The interactions in group 5 are interactions that restart the loop when the seconds reach the count that we desire.  When the loop is restarted, the following actions must be taken: Set ID_VAR_SECS and ID_VAR_SECS_1 to the initial value for the next loop ('0' in this case).  Note that ID_VAR_SECS_1 MUST be set before ID_VAR_SECS.  Additionally, if the loop is to continue, ID_VAR_SECS and ID_VAR_SECS_1 must be set to the same value.   ID_TEXT_SECONDS is set to the initial value.  If this isn't done, then the text box will try to animate from the final value to the initial value and then will look "weird". ID_VAR_END_CNT is reset to its initial value (60 in this case).  ID_BUTTON_SECS is also responsible for updating the minutes values.  In this case, it's incrementing the ID_TEXT_MINS value (counting up in minutes) and decrementing the ID_VAR_MIN_END_CNT  Adjusting the time of an animation object The animation object (as well as other emWin objects) use the GUI_X_DELAY function for timing.  It is up to the host software to implement this function.  In the i.MX RT examples, the General Purpose Timer (GPT) is used for this timer.  So how the GPT is configured will affect the timing of the application and the how fast or slow the animations run. The GPT is configured in the function BOARD_InitGPT() which resides in the main source file.  The recommended way to adjust the speed of the timer is by changing the divider value to the GPT. Conclusion So we have seen two different methods of implementing a real-time clock in an AppWizard GUI application.  Those methods are: Use an independent timer in your MCU Using animation objects Using an independent timer in your MCU may be preferred as it allows for better control over the timing, can allow for real-time actions to be performed that AppWizard can't control, and provides some assurance of precision.  Using animation objects may be preferred if you just need a quick timer implementation that doesn't require you to manually add code to your project or use a second timer.  
查看全文
Overview of i.MX RT1050         The i.MX RT1050 is the industry's first crossover processor and combines the high-performance and high level of integration on an applications processors with the ease of use and real-time functionality of a micro-controller. The i.MX RT1050 runs on the Arm Cortex-M7 core at 600 MHz, it means that it definitely has the ability to do some complicated computing, such as floating-point arithmetic, matrix operation, etc. For general MCU, they're hard to conquer these complicated operations.         It has a rich peripheral which makes it suit for a variety of applications, in this demo, the PXP (Pixel Pipeline), CSI (CMOS Sensor Interface), eLCDIF (Enhanced LCD Interface) allows me to build up camera display system easily Fig 1 i.MX RT series           It has a rich peripheral which makes it suit for a variety of applications, in this demo, the PXP (Pixel Pipeline), CSI (CMOS Sensor Interface), eLCDIF (Enhanced LCD Interface) allows me to build up camera display system easily Fig 2 i.MX RT1050 Block Diagram Basic concept of Compute Vision (CV)          Machine Learning (ML) is moving to the edge because of a variety of reasons, such as bandwidth constraint, latency, reliability, security, ect. People want to have edge computing capability on embedded devices to provide more advanced services, like voice recognition for smart speakers and face detection for surveillance cameras. Fig 3 Reason        Convolutional Neural Networks (CNNs) is one of the main ways to do image recognition and image classification. CNNs use a variation of multilayer perception that requires minimal pre-processing, based on their shared-weights architecture and translation invariance characteristics. Fig 4 Structure of a typical deep neural network         Above is an example that shows the original image input on the left-hand side and how it progresses through each layer to calculate the probability on the right-hand side. Hardware MIMXRT1050 EVK Board; RK043FN02H-CT(LCD Panel) Fig 5 MIMXRT1050 EVK board Reference demo code emwin_temperature_control: demonstrates graphical widgets of the emWin library. cmsis_nn_cifar10: demonstrates a convolutional neural network (CNN) example with the use of convolution, ReLU activation, pooling and fully-connected functions from the CMSIS-NN software library. The CNN used in this example is based on the CIFAR-10 example from Caffe. The neural network consists of 3 convolution layers interspersed by ReLU activation and max-pooling layers, followed by a fully-connected layer at the end. The input to the network is a 32x32 pixel color image, which is classified into one of the 10 output classes. Note: Both of these two demo projects are from the SDK library Deploy the neuro network mode Fig 6 illustrates the steps of deploying the neuro network mode on the embedded platform. In the cmsis_nn_cifar10 demo project, it has provided the quantized parameters for the 3 convolution layer, so in this implementation, I use these parameters directly, BTW, I choose 100 images randomly from the Test set as a round of input to evaluate the accuracy of this model. And through several rounds of testing, I get the model's accuracy is about 65% as the below figure shows. Fig 6 Deploy the neuro network mode Fig 7 cmsis_nn_cifar10 demo project test result The CIFAR-10 dataset is a collection of images that are commonly used to train ML and computer vision algorithms, it consists of 60000 32x32 color images in 10 classes, with 6000 images per class ("airplane", "automobile", "bird", "cat", "deer", "dog", "frog", "horse", "ship", "truck"). There are 50000 training images and 10000 test images. Embedded platform software structure         After POR, various components are initialized, like system clock, pin mux, camera, CSI, PXP, LCD and emWin, etc. Then control GUI will show up in the LCD, press the Play button will display the camera video in the LCD, once an object into the camera's window, you can press the Capture button to pause the display and run the model to identify the object. Fig8 presents the software structure of this demo. Fig 8 Embedded platform software structure Object identify Test The three figures present the testing result.   Fig 9 Fig 10 Fig 11 Furture work          Use the Pytorch framework to train a better and more complicated convolutional network for object recognition usage.
查看全文
Introduction i.MX RT ROM bootloader provides a wealth of options to enable user programs to start in various ways. In some cases, people want to copy application image from Flash or other storage device to SDRAM and run there. In this article, I record three ways to realize this. Section 2 and 3 shows load image from NOR flash. Section 4 shows load image from SD card. Software and Tools: MCUXpresso IDE v11.1 NXP-MCUBootUtility 2.2.0   MIMXRT1060-EVK   RT1060 SDK v2.7.0   Win10   Add DCD by MCUxpresso IDE If customers use MCUXpresso to develop the project, they can add DCD head by MCUXpresso. To show the work flow, we take evkmimxrt1020_iled_blinky as the example. Step 1: Add the following to Compiler options: XIP_BOOT_HEADER_DCD_ENABLE=1 SKIP_SYSCLK_INIT Step 2: Modify the Memory Configuration Step 3: Select link application to RAM Step 4. Compile the project. MCUXpresso will generate linker script automatically. Step 5. Since the code should be linked to RAM, MCUXpresso will not prefix IVT and DCD. We can add these link information to linker script manually. Add below code to .ld file’s head.     .boot_hdr : ALIGN(4)     {         FILL(0xff)         __boot_hdr_start__ = ABSOLUTE(.) ;         KEEP(*(.boot_hdr.conf))         . = 0x1000 ;         KEEP(*(.boot_hdr.ivt))         . = 0x1020 ;         KEEP(*(.boot_hdr.boot_data))         . = 0x1030 ;         KEEP(*(.boot_hdr.dcd_data))         __boot_hdr_end__ = ABSOLUTE(.) ;         . = 0x2000 ;     } >BOARD_SDRAM   Then deselect “Manage linker script” in last screenshot. Step 6. Recompile the project, IVT/DCD/BOOT_DATA will be add to your project. Then right click the project axf file->Binary Utilities->Create S-record.   After all these step, you can open MCUBootUtility and download the .s19 file to NOR flash.   Add DCD by MCUBootUtility We can also keep the linker script managed by IDE. MCUBootUtility can add head too. Sometimes it is more flexible than other manners. Step 1. This time BOARD_SDRAM location should be changed to 0x80002000 while the size should be 0x1cff000. This is because the start 8k space in bootable image is saved for IVT and DCD. Step 2. compile the project and generate the .s19 file. Step 3. Open MCUBootUtility. In MCUBootUtility, we should first set the Device Configuration Data. Here I use MIMXRT1060_EVK. So I select the DCD bin file in NXP-MCUBootUtility-2.2.0\src\targets\MIMXRT1062. After that, select the application image file and click All-in-one Action button. MCUBootUtility can do all the work without any manual operation.   Boot from SD card to SDRAM In some application, customer don’t want XIP. They want to use SD card to keep application image and run the code in RAM. But if the code size is bigger than OCRAM size, they have to copy image into SDRAM when startup. With MCUBootUtility’s help, this work is very easy too.  User just need to change the memory map which is located to 0x80001000.   In MCUBootUtility, select the Boot Device to “uSDHC SD” and insert SD card. Then connect the target board. If RT1060 can read the SD card, it will display the SD card information. Then same as last section, set the DCD file and application image file. Click the All-in-One Action button, MCUBootUtility will generate the bootable image and write it to SD card.   SD card has huge capacity. It's too wasteful to only store boot image. People may ask that can they also create a FAT32 system and store more data file in it? Yes, but you need tool's help. When booting from SD card, ROM code read IVT and DCD from SD card address 0x400. To FAT32, the first 512 bytes in SD is for MBR(MAIN BOOT RECORD). Data in address 0x1c6 in MBR reords the partition start address. If the space from MBR to partition start address is big enough to store boot image, then FAT32 system and boot image can live in peace. .   Conclusions:      To help Boot ROM initialize SDRAM, DCD must be placed at right place and indexed by IVT correctly. When our code seems not work, we should first check IVT and DCD.          The IVT offset from the base address for each boot device type is defined in the table below. The location of the IVT is the only fixed requirement by the ROM. The remainder or the image memory map is flexible and is determined by the contents of the IVT.
查看全文
Source code: https://github.com/JayHeng/NXP-MCUBootUtility   【v2.0.0】 Features: > 1. Support i.MXRT5xx A0, i.MXRT6xx A0 >    支持i.MXRT5xx A0, i.MXRT6xx A0 > 2. Support i.MXRT1011, i.MXRT117x A0 >    支持i.MXRT1011, i.MXRT117x A0 > 3. [RTyyyy] Support OTFAD encryption secure boot case (SNVS Key, User Key) >     [RTyyyy] 支持基于OTFAD实现的安全加密启动(唯一SNVS key,用户自定义key) > 4. [RTxxx] Support both UART and USB-HID ISP modes >     [RTxxx] 支持UART和USB-HID两种串行编程方式(COM端口/USB设备自动识别) > 5. [RTxxx] Support for converting bare image into bootable image >     [RTxxx] 支持将裸源image文件自动转换成i.MXRT能启动的Bootable image > 6. [RTxxx] Original image can be a bootable image (with FDCB) >     [RTxxx] 用户输入的源程序文件可以包含i.MXRT启动头 (FDCB) > 7. [RTxxx] Support for loading bootable image into FlexSPI/QuadSPI NOR boot device >     [RTxxx] 支持下载Bootable image进主动启动设备 - FlexSPI/QuadSPI NOR接口Flash > 8. [RTxxx] Support development boot case (Unsigned, CRC) >     [RTxxx] 支持用于开发阶段的非安全加密启动(未签名,CRC校验) > 9. Add Execute action support for Flash Programmer >     在通用Flash编程器模式下增加执行(跳转)操作 > 10. [RTyyyy] Can show FlexRAM info in device status >       [RTyyyy] 支持在device status里显示当前FlexRAM配置情况 Improvements: > 1. [RTyyyy] Improve stability of USB connection of i.MXRT105x board >     [RTyyyy] 提高i.MXRT105x目标板USB连接稳定性 > 2. Can write/read RAM via Flash Programmer >    通用Flash编程器里也支持读写RAM > 3. [RTyyyy] Provide Flashloader resident option to adapt to different FlexRAM configurations >     [RTyyyy] 提供Flashloader执行空间选项以适应不同的FlexRAM配置 Bugfixes: > 1. [RTyyyy] Sometimes tool will report error "xx.bat file cannot be found" >     [RTyyyy] 有时候生成证书时会提示bat文件无法找到,导致证书无法生成 > 2. [RTyyyy] Editing mixed eFuse fields is not working as expected >     [RTyyyy] 可视化方式去编辑混合eFuse区域并没有生效 > 3. [RTyyyy] Cannot support 32MB or larger LPSPI NOR/EEPROM device >     [RTyyyy] 无法支持32MB及以上容量的LPSPI NOR/EEPROM设备 > 4. Cannot erase/read the last two pages of boot device via Flash Programmer >    在通用Flash编程器模式下无法擦除/读取外部启动设备的最后两个Page
查看全文
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-342297
查看全文
Source code: https://github.com/JayHeng/NXP-MCUBootUtility 【v1.3.0】 Features: > 1. Can generate .sb file by actions in efuse operation utility window >    支持生成仅含自定义efuse烧写操作(在efuse operation windows里指定)的.sb格式文件 Improvements: > 1. HAB signed mode should not appliable for FlexSPI/SEMC NOR device Non-XIP boot with RT1020/1015 ROM >    HAB签名模式在i.MXRT1020/1015下应不支持从FlexSPI NOR/SEMC NOR启动设备中Non-XIP启动 > 2. HAB encrypted mode should not appliable for FlexSPI/SEMC NOR device boot with RT1020/1015 ROM >    HAB加密模式在i.MXRT1020/1015下应不支持从FlexSPI NOR/SEMC NOR启动设备中启动 > 3. Multiple .sb files(all, flash, efuse) should be generated if there is efuse operation in all-in-one action >    当All-In-One操作中包含efuse烧写操作时,会生成3个.sb文件(全部操作、仅flash操作、仅efuse操作) > 4. Can generate .sb file without board connection when boot device type is NOR >    当启动设备是NOR型Flash时,可以不用连接板子直接生成.sb文件 > 5. Automatic image readback can be disabled to save operation time >    一键操作下的自动程序回读可以被禁掉,用以节省操作时间 > 6. The text of language option in menu bar should be static and easy understanding >    菜单栏里的语言选项标签应该是静态且易于理解的(中英双语同时显示) Bugfixes: > 1. Cannot generate bootable image when original image (hex/bin) size is larger than 64KB >    当输入的源image文件格式为hex或者bin且其大小超过64KB时,生成可启动程序会失败 > 2. Cannot download large image file (eg 6.8MB) in some case >    当输入的源image文件非常大时(比如6.8MB),下载可能会超时失败 > 3. There is language switch issue with some dynamic labels >    当切换显示语言时,有一些控件标签(如Connect按钮)不能实时更新 > 4. Some led demos of RT1050 EVKB board are invalid >    /apps目录下RT1050 EVKB板子的一些LED demo是无效的 【v1.4.0】 Features: > 1. Support for loading bootable image into uSDHC SD/eMMC boot device >    支持下载Bootable image进主动启动设备 - uSDHC接口SD/eMMC卡 > 2. Provide friendly way to view and set mixed eFuse fields >    支持更直观友好的方式去查看/设置某些混合功能的eFuse区域 Improvements: > 1. Set default FlexSPI NOR device to align with NXP EVK boards >    默认FlexSPI NOR device应与恩智浦官方EVK板卡相匹配 > 2. Enable real-time gauge for Flash Programmer actions >    为通用Flash编程器里的操作添加实时进度条显示
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/community/imx/blog/2019/04/17/do-you-have-a-minute 
查看全文
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-342954
查看全文
This application note describes how to develop an H.264 video decoding application with the NXP i.MX RT1050 processor. Click here to access the full application note. Click here to access the github repo of FFMPEG(code, no GPL). state: the code is for evaluation purpose only.
查看全文
MCUXPRESSO SECURE PROVISIONING TOOL是官方今年上半年推出的一个针对安全的软件工具,操作起来非常的简单便捷而且稳定可靠,对于安全功能不熟悉的用户十分友好。但就是目前功能还不是很完善,只能支持HAB的相关操作,后续像BEE之类的需等待更新。 详细的介绍信息以及用户手册请参考官方网址:MCUXpresso Secure Provisioning Tool | Software Development for NXP Microcontrollers (MCUs) | NXP | NXP  目前似乎知道这个工具的客户还不是很多,大部分用的更多的还是MCU BOOT UTILITY。那么如果已经用了MCU BOOT UTILITY烧录了FUSE,现在想用官方工具了怎么办了?其实对两者进行研究对比后,他们最原始的执行部分都是一样的,所以我们按照如下步骤进行相应的简单替换就能把新工具用起来: 首先是crts可keys的替换, MCU BOOT UTILITY的路径是在: ..\NXP-MCUBootUtility-2.2.0\NXP-MCUBootUtility-2.2.0\tools\cst MCUXPRESSO SECURE PROVISIONING的对应路径是在对应workspace的根目录: 另外还有一个就是encrypted模式会用到的hab_cert,需要将下面这两个文件对应替换,而且两个工具的命名不同,注意修改。 MCU BOOT UTILITY的路径是在: ..\NXP-MCUBootUtility-2.2.0\NXP-MCUBootUtility-2.2.0\gen\hab_cert MCUXPRESSO SECURE PROVISIONING的路径是workspace里: ..\secure_provisioning_RT1050\gen_hab_certs MCU BOOT UTILITY里命名为:SRK_1_2_3_4_table.bin; SRK_1_2_3_4_fuse.bin MCUXPRESSO SECURE PROVISIONING里命名为:SRK_fuses.bin; SRK_hash.bin 至此,就能够在新工具上用起来了 最后提一下,就是这个新工具是可以建不同的workspace来相应存储不同秘钥的项目,能够方便用户区分。在新工具下建的项目也是可以互相替换秘钥的,参考上术步骤中的secure provisioning部分即可。
查看全文