uBLOX support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uBLOX support?

969 Views
mspenard603
Contributor IV

Hi All,

 Is there any example code to integrate a uBLOX (e.g., a NINA-W31 with its UART interface) with iMXRT and LWIP etc.?

Thanks

0 Kudos
Reply
1 Reply

874 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mike Spenard,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
There's no example code about the uBLOX wifi module in the i.MX RT's SDK library, however, in the SDK library, it contains the Lwip code demos.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply