rt1052 tw9990 issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rt1052 tw9990 issue

1,115 次查看
huangpeter
Contributor II

rt1052    Release Name: MCUXpresso Software Development Kit (SDK)
Release Version: 2.4.2

I have done below procedure:
1, tw9990 i2c driver work fine, and config to ccir565 mode.
2, data pin[0:7], pclk connect to rt1050  csi[2:9]. 
3, refer to adv1780 patch for i.mx6ul, added csi patch.
4, tw9990 connect to PAL(720X576) CCIR656 Interlace Mode camera.

but camera preivew app does not work 

csiBase->CSICR1 9190504

csiBase->CSICR2 40000000

csiBase->CSICR3 21003

csiBase->CSISTATFIFO 0

csiBase->CSIRFIFO af80af80

csiBase->CSIRXCNT 9600

csiBase->CSISR 82204001

csiBase->CSIDMASA_STATFIFO 0

csiBase->CSIDMATS_STATFIFO 0

csiBase->CSIDMASA_FB1 80000080

csiBase->CSIDMASA_FB2 80195080

csiBase->CSIFBUF_PARA b4

csiBase->CSIIMAG_PARA 5a00240

csiBase->CSICR18 80080234

csiBase->CSICR19 4

标签 (1)
0 项奖励
回复
1 回复

947 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Peter,

DFAE Evan reported this issue with case number: 00195780.

I am checking with i.MX RT product team about this issue.

I will reply at case: 00195780

Thank you for the understanding.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复