Dear all,
I am using mbedtls libraries for tls connection . i connected with my pc broker it is connecting and publishing. if i connected with any other pc broker with same certificates it is not connected .In wireshark, while handshaking (after server hello done) i am getting alert message .
if i connected with my broker pc in terminal i am getting this message,
mqtt client is connected
protocol version TLS1.2
ciphersuite is TLS_ECDHE_RSA_WITH_AES_128_GCM_SHA256
if i connected with any other pc in terminal i am getting this message,
mqtt client is not connected
protocol version SSLV3.0
ciphersuite is
Hi asvitha,
I don't know which NXP chip you are using, do you use the RT chip?
If yes, do you test the NXP SDK code, take RT1060 as an example:
SDK_2.8.6_EVK-MIMXRT1060_freertos\boards\evkmimxrt1060\mbedtls_examples
Do you try that code? Whether it works for your or not?
You also can check:
SDK_2.8.6_EVK-MIMXRT1060_freertos\boards\evkmimxrt1060\lwip_examples\lwip_httpssrv_mbedTLS
SDK_2.8.6_EVK-MIMXRT1060_freertos\boards\evkmimxrt1060\lwip_examples\lwip_httpscli_mbedTLS
The related code all has the readme.txt, you can follow it, thanks.
Best Regards,
Kerry