Hi
Inside MCUXpresso there is complete project for flashdriver QSPI with imxrt1050 microprocessor. I need to use a flashdriver for imxrt1060. I use NOR memory with QSPI. I know inside mcuxpresso there is a driver ( *.cfx file) for imxrt1060 but I didn't find the project.
Could anyone send me the project to get cfx file with imxrt1060 microprocessor?
Thank you
Best Regads
Giovanni Grondona
Hello,
One can refer to the imxrt1050 project. It is ok for the imxrt1060. Hope it help you.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------