imxrt1060 flash driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1060 flash driver

897 Views
giannigrondona
Contributor III

Hi

Inside MCUXpresso there is complete project for flashdriver QSPI with imxrt1050 microprocessor. I need to use a flashdriver for imxrt1060. I use NOR memory with QSPI. I know inside mcuxpresso there is a driver ( *.cfx file) for imxrt1060 but I didn't find the project.

Could anyone send me the project to get cfx file with imxrt1060 microprocessor?
Thank you

Best Regads

Giovanni Grondona

Labels (1)
0 Kudos
Reply
1 Reply

787 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One can refer to the imxrt1050 project. It is ok for the imxrt1060. Hope it help you.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply