iMXRT1050 - Enhanced LCD Interface (Outstanding Requests)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1050 - Enhanced LCD Interface (Outstanding Requests)

808件の閲覧回数
jh1
Contributor III

Hi,

i have a question regarding the LCDIF General Control2 Register.

We had to modify the OUTSTANDING_REQS bitfield from REQ_2 to REQ_8 in order to avoid screen shifts.

In the RM it says: "This bitfield indicates the maximum number of outstanding transactions that LCDIF should request when it is acting as a bus master."

What does that mean exactly?

What is requested?

How do 2 and 8 outstanding requests differ?

Thanks,

Johann

タグ(2)
0 件の賞賛
返信
1 返信

756件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Johann,

 

Please also see this thread: https://community.nxp.com/thread/443873 

Outstanding transactions refer to data and commands.

 

Best regards,

Felipe

0 件の賞賛
返信