i.MXRT 1052 porting - sl_IfStartWriteSequence and sl_IfEndWriteSequence APIs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT 1052 porting - sl_IfStartWriteSequence and sl_IfEndWriteSequence APIs

931件の閲覧回数
suhel_mulla
Contributor III

I am working of Freertos based LPUART example from SDK on  NXP i.MXRT 1050 EVK board .

I have following queries - 

1. Is their any document / post having detailed dexplanation of LPUART_RTOS_Receive(lpuart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received) API. If not, can anybody explain it here?

2. What is the difference between ring buffer overflow & hardware buffer overflow?

3. When hardware buffer overflow occurs?

ラベル(4)
0 件の賞賛
返信
1 返信

893件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Suhel,

In order to keep the information in one place. Please refer to your other post for the above answers:

https://community.nxp.com/thread/538926 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信