i.MX RT1170 using MIPI to drive HDMI LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1170 using MIPI to drive HDMI LCD

1,768件の閲覧回数
auftrag2021
Contributor III

maybe it is a stupid question:

I want to use the i.MXRT1170 EVK MIPI interface to drive some LCD with standard HDMI. 

What is the "easiest" way to realize it?

Does NXP have some recommendated MIPI -> HDMI adapter board to purchase?

0 件の賞賛
返信
3 返答(返信)

1,657件の閲覧回数
kfw1972
Contributor I

Hi Auftrag2021 - just to give you a run down on my solution at the moment: MIPI DSI -> eDP converter chip using TI's sn65dsi86. Then you can use an adaptor cable from eDP to HDMI.   

タグ(1)
0 件の賞賛
返信

1,669件の閲覧回数
kfw1972
Contributor I
Hi Auftrag2021 - I want to do the same! Did you have any success finding a solution?
0 件の賞賛
返信

1,759件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello auftrag2021,

Good question! There is not a reference design or module for the i.MXRT1170 specifically, but there is a MIPI to HDMI adapter as part of the i.MX8 Accessory Boards which may serve as a general reference if you want to implement something similar. (The i.MX8 accessory board is not compatible as it uses a different connector).

The schematic for this adapter is available on the link below (you may need to login to download these design files). As you will see, it uses a ADV7535 which provides a MIPI/ DSI input receiver and a High-HDMI transmitter output.

https://www.nxp.com/webapp/Download?colCode=IMX-MIPI-HDMI&appType=license

I hope that this information helps!

Regards,
Gustavo

0 件の賞賛
返信