i.MX RT1064 EVK altium files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1064 EVK altium files

1,369 Views
sagonzal
Contributor III

I have purchased the i.MX RT1064 EVK and would like to examine the PCB layout however I exclusively use Altium and I cannot import the design files which are in Cadence Allegro format. Would it be possible to obtain a copy of the design files for this PCB in Altium format please?

Thanks

0 Kudos
Reply
3 Replies

1,340 Views
sagonzal
Contributor III

Thanks for your prompt reply Felipe. I'm only needing the i.MX part, if you give it to my in OrCAD file format is ok.

I mean the library of the schematic component your guys are using, that is the only file I need to include the RT1064 in my new PCB design.

Kind regards

0 Kudos
Reply

1,327 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

I sent you an email, please check it.

 

0 Kudos
Reply

1,353 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, we only provide these files in OrCAD format. Sorry for the inconvenience.

Best regards,

Felipe

0 Kudos
Reply