i.MX RT1064 EVK altium files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1064 EVK altium files

1,326件の閲覧回数
sagonzal
Contributor III

I have purchased the i.MX RT1064 EVK and would like to examine the PCB layout however I exclusively use Altium and I cannot import the design files which are in Cadence Allegro format. Would it be possible to obtain a copy of the design files for this PCB in Altium format please?

Thanks

0 件の賞賛
返信
3 返答(返信)

1,297件の閲覧回数
sagonzal
Contributor III

Thanks for your prompt reply Felipe. I'm only needing the i.MX part, if you give it to my in OrCAD file format is ok.

I mean the library of the schematic component your guys are using, that is the only file I need to include the RT1064 in my new PCB design.

Kind regards

0 件の賞賛
返信

1,284件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

I sent you an email, please check it.

 

0 件の賞賛
返信

1,310件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, we only provide these files in OrCAD format. Sorry for the inconvenience.

Best regards,

Felipe

0 件の賞賛
返信